cancel
Showing results for 
Search instead for 
Did you mean: 

Using multiple SPI slaves on the single SPI bus.

ASing.15
Associate II

Is there any available example or threads for using multiple SPI slaves on the single SPI bus?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

Which chip?

Multiple slaves is conceptually quite similar to a single slave. Use a different CS pin for each slave and toggle them as you want to talk to each chip.

If you feel a post has answered your question, please click "Accept as Solution".
ASing.15
Associate II

Thanks for replying.

I have STM32L496ZG.

I am specifically looking for SPI flash as one of the SPI slaves in multiple SLAVE scenarios on the single SPI bus.