2024-05-02 6:39 AM
Hi,
I have been trying to connect PSRAM and NOR FLASH to STM32H563 nucleo board using Dual-Quad-SPI.
I was able to successfully read/write to PSRAM and NOR Flash individually in single-Quad-SPI mode with base address 0x90000000. i'm not clear how the addressing is taken care, when we connect both PSRAM and NOR Flash in dual-Quad-SPI mode.
2024-06-06 5:29 AM - edited 2024-06-06 5:29 AM
Thanks for your information. I just want to know one more information like how the memory mapped mode is used. I want both flash and RAM memories should be considered as internal memory. Is it having two different addresses for memory mapping?