cancel
Showing results for 
Search instead for 
Did you mean: 

Use LPTIM for the period measure.

FRest.1
Associate III

I've clear (or at least I think so) how to use the timers (TIM), with "Input capture direct mode", in order to measure a period of one input pulse, but I don't understand how to do the same measure with the low power timer (LPTIM). The LPTIM associated with an external source seems dedicated to counting events.

I need one (o more) example, but all I found is TIM-related.

Can I have any help?

Grazie.

F.

2 REPLIES 2

Unfortunately, LPTIM is not equipped with input capture nor similar mechanism, so you cannot measure period of a signal.

JW

FRest.1
Associate III

Ma che tristezza. :(