cancel
Showing results for 
Search instead for 
Did you mean: 

USB_OTG_FS on the STM3240G-EVAL?

mattscar
Associate II
Posted on August 21, 2013 at 01:04

I can't get USB_OTG_FS communication to work on the STM3240G-EVAL board. USB_OTG_HS works with no problem. I tried disabling HS using JP31, but ST's example application still can't reach the USB_OTG_FS.

I thought this might be caused by a defective board, but the second board we bought has the same problem. So I suspect there's a simple reason for this. Has anyone gotten this to work?
2 REPLIES 2
Posted on August 21, 2013 at 02:34

Don't have the board, but would suggest you try and compile some of the other example projects in the USB FW library.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mattscar
Associate II
Posted on August 21, 2013 at 03:49

I downloaded the USB Host-Device Library from ST and compiled the MSC example for USB devices. But when I loaded it onto the board, the OTG_FS connection didn't respond. I used the following flags: -DUSE_STDPERIPH_DRIVER=1 -DSTM32F4XX=1 -DUSE_STM324xG_EVAL=1 -DUSE_USB_OTG_FS=1

My USB protocol analyzer tells me that the device simply timed out. Well, at least the OTG_FS connection on the Discovery board works.