2009-11-11 10:04 PM
USB mass storage with Linux and OS-X
2011-05-17 04:29 AM
Hi everybody,
Does anybody try to use the USB mass storage system under Linux and OS-X environments ? In our case, the first trials do not work properly. The OS see the structure of the media but after that, nothing is working properly. For example, the data files retrieved from the media is full of 0. Any comment is welcome as we are lost in our analysis. Best regards, HLI2011-05-17 04:29 AM
Hi hli,
I am using USB mass storage, demonstration with Linux(2.6.5) and STM3210E-EVAL board, to read/write sdcards. attached is a short log. >> SD card file system is FAT32'' regards, G.Ab. [ This message was edited by: g-ab on 12-11-2009 11:38 ]