Posted on May 17, 2011 at 13:37Hello, I suppose that maybe there is an overwrite of ''rawdata'' partition, can you check that the new ''rootfs.img.bin'' fit in ''rootfs'' partition. /* * 0x00000000-0x00100000 : ''Kernel raw data'' * 0x00100000-0x0...
Posted on May 17, 2011 at 13:37Hello! To use GDB with STM3210E-EVAL you need to have gdbserver in the target file system. It can be included from uClinux distribution Configuration menu. Also as I see there is only one serial port initialized to han...
Posted on May 17, 2011 at 13:32Hi, >> ''/bin/sh: cc: command not found '' try to type cc -v in your shell to see if a gnu c compiler exist in your path. Try to install ''c development'' & ''kernel development'' packages from your fedora installation...
Posted on May 17, 2011 at 13:29Hi hli, I am using USB mass storage, demonstration with Linux(2.6.5) and STM3210E-EVAL board, to read/write sdcards. attached is a short log. >> SD card file system is FAT32'' regards, G.Ab. [ This message was edited b...
Posted on May 17, 2011 at 13:26Quote:On 15-10-2009 at 10:50, Anonymous wrote: hello.my project involves using stm32-p103 board.i have downloaded and installed the toolchain from codesouecery from http://www.codesourcery.com/sgpp/lite/arm/portal/re...