2011-12-17 7:55 AM
Hi,
according to datasheet, it should be possible to get data transfer rates in the range of 50MByte/sec from SDIO interface to USB_HI port. Is there any example available? I would like to test, whether this would work for my application (ST32F4 USB in device mode, transferring data from a AD converter to a connected PC). But I think I have no possibility without some working example (in fact I would best need a firmware ST32F4 example PLUS a PC software example, best in Visual C. I would already be happy for some Bulk In-Out example (sort of loop-back-example - so WITHOUT using SDIO interface). Anybody has any idea where I could get such an example?