2016-03-01 3:07 PM
I am using the Stm32CubeL4 to generate a USB device with a CDC class. This is on a custom board. I am not using the USB ID line or VBUS.
It runs, but USBD_CDC_Init() is never called. On the Windows side, I see an ''unknown device'' with message ''Windows has stopped this device because it has reported problems. (Code 43)''. All driver items are marked as unknown. I tried upgrading the driver it said none found. I installed stsw_stm32102 the Virtual Com driver but the problem continues. I suspect there is a low level USB problem that occurs prior to getting the VID/DID, I have not seen the USB become addressed yet. I have not added any code to send or receive data over the port yet or to handle any events. I also bumped the heap size to 400 to no avail. Is there a way to debug the USB interface with Windows and find the cause of the problem? TIA, Jan #o2016-03-04 1:02 PM