usart3 remapping
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2009-10-22 1:28 AM
usart3 remapping
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 4:26 AM
I do not succeed in 'half' remapping the USART3 on a STM32F103RB device (64LQFP, 128K Flash/20K RAM)
The software works when port 3 in not remapped (with I2C2 clock disabled) and uses the same code as for port 1 and 2. The pins PC10 and PC11 can be toggled when used as push pull output. Has anyone experienced a similar problem or can just advice me in what to do next ? Thanks in advance. The code below shows the only difference between remap or not by means of the definition of 'USART3_PartialRemap'. #ifdef USART3_PartialRemap /* Configure USART3 Rx (PC.11) as input floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Configure USART3 Tx (PC.10) as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinRemapConfig( GPIO_PartialRemap_USART3, ENABLE ); #else /* Configure USART3 Rx (PB.11) as input floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOB, &GPIO_InitStructure); /* Configure USART2 Tx (PB.10) as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); #endif RCC_APB1PeriphClockCmd( RCC_APB1Periph_USART3, ENABLE);- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 4:26 AM
I'm using USART3 in partial remap mode, also using flow control on a STM32F103RET6 (64LQFP, 512K/64K). Initialization code is similar to yours, I have the remap statement before the GPIO init. I have a GSM modem attached, works fine.
Would look at GPIO-C clock. For the flow control to work you have to park the CAN controller off the RTS/CTS pins, otherwise it interferes with the operation (see errata) Finally after configuring the pins, enable the clock, then the USART .. else if (Uart->Port == USART3) { /* Enable USART3 Clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE); } USART_Cmd(Uart->Port, ENABLE); /* Enable the USART */ .. What is the failure mode? Do you not see data on the Tx pin? Is the USART taking data and do you see the registers/status reflect changing internal state? -Clive- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 4:26 AM
Dear Clive,
Thanks for your response. I tried on a 'RET6' device too and I have the same problem. The GPIO clocks are enabled, otherwise I would be able to toggle the pins via JTAG. I also tried the remap statement before and after. But in the next coming days I'll try some other things you propose. regards, Koen- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 4:26 AM
AFIO clock?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 4:26 AM
Domen,
Thank you very much. Now it works.