Posted on May 17, 2011 at 13:26Dear Clive, Thanks for your response. I tried on a 'RET6' device too and I have the same problem. The GPIO clocks are enabled, otherwise I would be able to toggle the pins via JTAG. I also tried the remap statement bef...
Posted on May 17, 2011 at 13:26I do not succeed in 'half' remapping the USART3 on a STM32F103RB device (64LQFP, 128K Flash/20K RAM) The software works when port 3 in not remapped (with I2C2 clock disabled) and uses the same code as for port 1 and 2....
Posted on May 17, 2011 at 13:26Dear, I think if you search at TI for examples you should find something and maybe by just adjusting the hardware layer and compile it for STM32 it could work if written in C. Maybe search also the older devices for ex...