Posted on May 17, 2011 at 13:34Floating GPIOs come to mind. They should either be output set to some value, pull-up/down input or analog input. More info is found on this forum, there's also a FAQ entry, I think.
Posted on May 17, 2011 at 13:32> For STM32 MCUs, ST-LINK is driven by the Atollic toolset, TrueSTUDIO (version 1.0 or later), IAR toolset EWARM (version 5.30 or later) and Keil toolset ARM-MDK (version 3.3 or later). And atollic seems to be based on...
Posted on May 17, 2011 at 13:30SPI_InitStructure.SPI_CPOL = SPI_CLOCK_POL; SPI_InitStructure.SPI_CPHA = SPI_MODE_1; Where are these defines from? in my spi.h, there's: #define SPI_CPOL_Low ((u16)0x0000) #define SPI_CPOL_High ((u16)0x0002) #define SP...
Posted on May 17, 2011 at 13:27amontec, olimex and some other companies make usb dongles that cost around 50eur Heh, ok, it was an old message for which I forgot to ''send''. On prices - olimex doesn't include VAT, for amontec you'll probably pay cu...