2022-07-12 9:56 AM
Hello,
I am struggling to use multiple USARTs. I tested that USART2 works fine but I cannot get USART1 and USART3 to work.
If I can't use multiple USARTs at the same time, I would like to use only USART3. However, USART3 does not work. Do I need to change settings on the Windows to use different USART?
I am using STM32F446 nucleo board and using Putty to see serial port on windows.
Any help would be very appreciated!
Thank you
void SendInitString(void)
{
uint8_t Test3[] = "Hello World 33 !!!\r\n"; //Data to send
HAL_UART_Transmit(&huart3,Test3,sizeof(Test3),10);// Sending in normal mode
uint8_t Test2[] = "Hello World 22 !!!\r\n"; //Data to send
HAL_UART_Transmit(&huart2,Test2,sizeof(Test2),10);// Sending in normal mode
uint8_t Test1[] = "Hello World 11 !!!\r\n"; //Data to send
HAL_UART_Transmit(&huart1,Test1,sizeof(Test1),10);// Sending in normal mode
HAL_Delay(1000);
}
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_USART2_UART_Init();
MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
SendInitString();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
Solved! Go to Solution.
2022-07-13 1:19 AM
@LCho.1 "The solution was to connect tx and rx of usart3 to FTDI cable"
Not sure what you mean by that - please explain further?
Obviously, the ST-Link's VCP on the Nucleo board is hardwired to 2 pins on the STM32 - this is explained in the documentation, and you can see it in the schematics.
The VCP can only connect to one UART at a time.
So, if you want to use a different UART, you'd have to
2022-07-12 12:35 PM
The solution was to connect tx and rx of usart3 to FTDI cable, not rely only on the usb cable connected to the nucleo board
2022-07-13 1:19 AM
@LCho.1 "The solution was to connect tx and rx of usart3 to FTDI cable"
Not sure what you mean by that - please explain further?
Obviously, the ST-Link's VCP on the Nucleo board is hardwired to 2 pins on the STM32 - this is explained in the documentation, and you can see it in the schematics.
The VCP can only connect to one UART at a time.
So, if you want to use a different UART, you'd have to