cancel
Showing results for 
Search instead for 
Did you mean: 

Device firmware upgrade pins in STM32F303ZET6 are USART1 (PA9/PA10), USART2 (PA2/PA3) or USB (PA11/PA12).But my external interface is UART. Can i able to configure the USART pins as UART?

KJ.4
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
gbm
Principal

USART is UART. You don't need to configure anything. The bootloader works out of the box.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
waclawek.jan
Super User

> USART is UART

... with synchronous capability (hence the S), which is not used in the bootloader, as gbm said above.

JW

The ROM supports what it supports, the functionality described in AN2606 is what is available, and the pins it uses.

The protocol uses asynchronous 8E1 serial data, it's not using synchronous modes, there is not a clock signal

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..