cancel
Showing results for 
Search instead for 
Did you mean: 

USART with DMA circular buffer transfer only the first byte

Emanuele Zampieri
Associate II

Hello,

I have to transfer the bytes received from UART2 to the circular buffer via DMA. The microcontroller I am using is STM32L010F4  with LL instead of HAL.

When I send a sequence of bytes to UART2 I notice that only the first byte is loaded into the buffer and the UART IDLE interrupt is triggered.

Every time I send a sequence of bytes the IDLE interrupt is triggered but in the buffer I always see only the first byte.

Thanks!

#define ARRAY_LEN(x)            (sizeof(x) / sizeof((x)[0]))
 
DMADataCallback _dataCallback;
static uint8_t _usartRxDmaBuffer[64];
/* USER CODE END 0 */
 
/* USART2 init function */
 
void USART_Init(DMADataCallback callback)
{
	_dataCallback = callback;
	
	LL_USART_InitTypeDef USART_InitStruct = {0};
  LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
 
  /* Peripheral clock enable for UART and DMA */
  LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_USART2);
  LL_IOP_GRP1_EnableClock(LL_IOP_GRP1_PERIPH_GPIOA);
  LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_DMA1);
	
	/**
	* USART2 GPIO Configuration  
  * PA2   ------> USART2_TX
  * PA3   ------> USART2_RX 
  */
  GPIO_InitStruct.Pin = LL_GPIO_PIN_2;
  GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
  GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
  GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
  GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
  GPIO_InitStruct.Alternate = LL_GPIO_AF_4;
  LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
  GPIO_InitStruct.Pin = LL_GPIO_PIN_3;
  GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
  GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
  GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
  GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
  GPIO_InitStruct.Alternate = LL_GPIO_AF_4;
  LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
  /* USART2 DMA init */
  LL_DMA_SetPeriphRequest(DMA1, LL_DMA_CHANNEL_3, LL_DMA_REQUEST_4);
  LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_3, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
  LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_3, LL_DMA_PRIORITY_VERYHIGH);
  LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_3, LL_DMA_MODE_CIRCULAR);
  LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_3, LL_DMA_PERIPH_NOINCREMENT);
  LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_3, LL_DMA_MEMORY_INCREMENT);
  LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_3, LL_DMA_PDATAALIGN_BYTE);
  LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_3, LL_DMA_MDATAALIGN_BYTE);
 
  LL_DMA_SetPeriphAddress(DMA1, LL_DMA_CHANNEL_3, (uint32_t)&USART2->RDR);
  LL_DMA_SetMemoryAddress(DMA1, LL_DMA_CHANNEL_3, (uint32_t)_usartRxDmaBuffer);
  LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_3, ARRAY_LEN(_usartRxDmaBuffer));
 
  /* Enable HT & TC interrupts */
  LL_DMA_EnableIT_HT(DMA1, LL_DMA_CHANNEL_3);
  LL_DMA_EnableIT_TC(DMA1, LL_DMA_CHANNEL_3);
 
  /* DMA interrupt init */
  NVIC_SetPriority(DMA1_Channel2_3_IRQn, 0);
  NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);
 
  /* USART2 configuration */
  USART_InitStruct.BaudRate = 115200;
  USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
  USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
  USART_InitStruct.Parity = LL_USART_PARITY_NONE;
  USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
  USART_InitStruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
  USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
  LL_USART_Init(USART2, &USART_InitStruct);
  LL_USART_ConfigAsyncMode(USART2);
  LL_USART_EnableDMAReq_RX(USART2);
  LL_USART_EnableIT_IDLE(USART2);
 
  /* USART interrupt */
  NVIC_SetPriority(USART2_IRQn, 0);
  NVIC_EnableIRQ(USART2_IRQn);
 
  /* Enable USART and DMA */
  LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_3);
  LL_USART_Enable(USART2);
}
 
/* USER CODE BEGIN 1 */
void DMA_RX_Check(void) 
{
	static size_t old_pos;
  size_t pos;
 
  /* Calculate current position in buffer */
  pos = ARRAY_LEN(_usartRxDmaBuffer) - LL_DMA_GetDataLength(DMA1, LL_DMA_CHANNEL_3);
  if (pos != old_pos) 
	{	/* Check change in received data */
		if (pos > old_pos) 
		{	/* Current position is over previous one */
			/* We are in "linear" mode */
      /* Process data directly by subtracting "pointers" */
      _dataCallback(&_usartRxDmaBuffer[old_pos], pos - old_pos);
    } 
		else 
		{
			/* We are in "overflow" mode */
			/* First process data to the end of buffer */
			_dataCallback(&_usartRxDmaBuffer[old_pos], ARRAY_LEN(_usartRxDmaBuffer) - old_pos);
			/* Check and continue with beginning of buffer */
			if (pos > 0) 
				_dataCallback(&_usartRxDmaBuffer[0], pos);
    }
	}
  old_pos = pos;	/* Save current position as old */
 
  /* Check and manually update if we reached end of buffer */
  if (old_pos == ARRAY_LEN(_usartRxDmaBuffer))
		old_pos = 0;
}
void DMA1_Channel2_3_IRQHandler(void)
{
	/* Check half-transfer complete interrupt for DMA1 (UART2) */
  if (LL_DMA_IsEnabledIT_HT(DMA1, LL_DMA_CHANNEL_3) && LL_DMA_IsActiveFlag_HT3(DMA1)) {
      LL_DMA_ClearFlag_HT3(DMA1);	/* Clear half-transfer complete flag */
      DMA_RX_Check();						/* Check for data to process */
  }
 
  /* Check transfer-complete interrupt for DMA1 (UART2) */
  if (LL_DMA_IsEnabledIT_TC(DMA1, LL_DMA_CHANNEL_3) && LL_DMA_IsActiveFlag_TC3(DMA1)) {
      LL_DMA_ClearFlag_TC3(DMA1);	/* Clear transfer complete flag */
      DMA_RX_Check();						/* Check for data to process */
  }
}
 
void USART2_IRQHandler(void)
{
	/* Check for IDLE line interrupt */
  if (LL_USART_IsEnabledIT_IDLE(USART2) && LL_USART_IsActiveFlag_IDLE(USART2)) {
		LL_USART_ClearFlag_IDLE(USART2);	/* Clear IDLE line flag */
    DMA_RX_Check();									/* Check for data to process */
  }
}

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User
17 REPLIES 17
TDK
Super User

How do you know the line doesn't go idle between characters?

If you feel a post has answered your question, please click "Accept as Solution".

I analyzed TX and RX with a logic analyzer

waclawek.jan
Super User

If you observe the UART registers in debugger, then don't.

Otherwise, read out and check/post the DMA registers content before and after the data packet, together with the expected and actual content of the buffer in memory.

JW

In debug I only observe the contents of the circular buffer used by the DMA (_rxDataCallback).

In the circular buffer only the first byte of the sequence (C0 10 00 05 43 C0) I send is stored.

0693W000003Oh1bQAC.png0693W000003Oh3cQAC.png

I tried to view the memory contents by activating the "live update" or inserting a breakpoint, in the buffer I always see only the first byte.

waclawek.jan
Super User

Read out and check/post the DMA registers content before and after the data packet.

JW

waclawek.jan
Super User

Also, have you tried to receive the same stream using simple polling?

Isn't the overrun flag set in USART?

What's the baudrate and what's the system clock?

JW

Emanuele Zampieri
Associate II

Sorry, maybe i didn't attach pictures correctly before.

The contents of the DMA registers remain the same after sending the packet.

0693W000003OikXQAS.jpg

I was already checking the ORE flag and in debugging I see that after sending the packet this flag is raised.

The USART2 baudrate is set to 115200 and the clock is set as in the image:

0693W000003OitFQAS.jpg

waclawek.jan
Super User

> I was already checking the ORE flag and in debugging I see

> that after sending the packet this flag is raised.

Then that is the problem.

Didn't data arrive before DMA is set?

Isn't there something interfering with DMA?

Write a minimal program with only the UART and DMA and nothing else. Still the same problem?

JW

MM..1
Chief III

Try check if this realy work

#define ARRAY_LEN(x) (sizeof(x) / sizeof((x)[0]))