cancel
Showing results for 
Search instead for 
Did you mean: 

USART1 problem to setup without configurator

VSimo.18
Associate II
Hi at everyone,
I need to write a code without the Cube IDE configurator, due to save program memory. I tryed to configure the USAR1, but seem not output on the pin the data streem. Seem that the machine runs because, at the first, I tryed to transmit in polling mode cheching the TXE flag to charge the the TDR register, but not data goes to the pin, but rather, the TX pin seem on high impedence. I forgot something.
Below the USART init :
RCC_CCIPR &= 0xfffffffc; //USART1 clock on system clock RCC_APBENR2 |= 0x00004000; //USART1 clock enable RCC_IOPENR |= 0x00000005; //GPIOC clock enable PORTC_MODER &= 0xefffffff; //set PC14 as alternate function PORTC_AFRH &= 0xf0ffffff; //set PC14 as TxD function PORTC_OTYPER &= 0xffffbfff; //PC14 PP mode USART1_CR1 |= 0x00000001; //USART1 enabled USART1_CR1 &= 0xefffefff; //8 bit data length USART1_CR3 = 0x00002000; //DMA disable USART1_BRR = 0x000001a1; //115200 USART1_CR1 |= 0x00000008; //TX enabled // USART1_CR1 |= 0x00000004; //RX enabled The TXD pin is on GPIOC14 then into the main program call every 1 second the follow procedure: void uart_polling_send(const uint8_t *pData, uint16_t Size, uint16_t Timeout) { const uint8_t *pdata8bits; pdata8bits = pData; //USART1_CR1 |= 0x00000008; //TX enabled while(Size > 0U) { PORTC_ODR ^= 0x8000; while((USART1_ISR & 0x00000080) == 0) //check TXE flag { //here will manage the timeout } USART1_TDR = (uint8_t)(*pdata8bits & 0xFFU); pdata8bits++; Size--; } while((USART1_ISR & 0x00000040) == 0) //check TC flag { //here will manage the timeout } }
View more
Using the "PORTC_ODR ^= 0x8000;" instuction I can check how many time execute and how is the execution time (using an oscilloscope). Seem works the flow into the procedure, but as I say the peripheral pin not work. Why?
Thank you at all!
Valter

 

8 REPLIES 8
Andrew Neil
Super User

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution; in particular How to insert source code.

You haven't said what chip you're using, or what board it's on.

Please also show the complete code.

 


@VSimo.18 wrote:
I need to write a code without the Cube IDE configurator, due to save program memory.

Have you tried with the configurator first ?

You could take that as your basis, and then optimise it if required...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Dump the registers for GPIOx and RCC, so you know what's in them

Don't use RMW on the SAME register on multiple lines, it's NOT efficient

Use USART1_CR1 = (USART1_CR1 & ~clear_bits) | set_bits; // so the compile can fold the operation

Don't immediately touch the peripheral who's clock you've enabled, reorder things, say enable GPIOA/GPIOC clocks, then USART1 clock, then touch GPIOC->xx registers, so you've given the pipeline/write-buffer a chance to work.

Correctly comment the lines

Initialize PC15 properly as a OUTPUT-PP, be aware PC13..15 have LOW CURRENT drivers

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi Andrew,
yes I tryed with configurator and works, but the code to big.
the coplete code is the main file into it is called the USART1_init, and after into the "while(1)" is called the uart_polling_send to send data out of the USART.
could you see any mistake o maybe some lacke in the init flow. I read the data sheet more then one time and I verified to need
enable USART cloc,.
enable GPIOC clock,
select USART clock on SYSClock is on default, but I forced it in any case,
select PC14 as alternate function.
select AF0 (USART1),
select PC14 as push-pull (I don't know if necessary),
enable UART1,
set USART1 without fifo,
enable TX.....

but the PC14 stays on high inpedenze.
Notice, if I comment the "select PC14 as alternate function", it possible to drive the PC14 writing on ODR register, otherwise PC14 isn't driven. Seem the select PC14 as alternate function works, bat because the fisical pin is on high inpedence? I don't understud.

Note:

Thank you of "Please see How to write your question to maximize your chances to find a solution; in particular How to insert source code.", and sorry.

Valter

 

0x4000 would be PC14

0x8000 is PC15, ie (1 << 15)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@VSimo.18 wrote:

yes I tryed with configurator and works,


So compare & contrast what your code does against what the conifgurator's code does.

Or just take the configurator's code, and cut it down to your requirements.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Yes I use UART1_TX on PC14.

I try to follow your previous advises.

Valter

Yes I thinked to do in this way, but it is the first time that I use a STM and the CUBE, and it is not frendly for me, instede I use to use directly the registers (on Renesas, Microchip and Motorola, in the past, 32 bits MCU).
In the project builded with the configurator I send all the registers value to the USART, and seem are the same that I set "manually".
But as I said into the polling procedure seem to works correctly, as the clock is preset and the registers are correct. That is very strange is that the TX pin, connected to the oscilloscope, not show anyting, rather if touched by finger show as it is high impedenze. As if it is not connected to the peripheral.

Valter

VSimo.18
Associate II

Update guys,
I tryed the change suggested from Tesla, but no effect I saw.

RCC_IOPENR |= 0x00000005; //GPIOA & GPIOC clock enable RCC_CCIPR &= 0xfffffffc; //USART1 clock enable on system clock RCC_APBENR2 |= 0x00004000; //USART1 clock enable HAL_Delay(100); //USART1_CR1 |= 0x00000001; //USART1 enabled USART1_CR1 = USART1_CR1 | 0x00000001; //USART1 enabled USART1_CR1 &= 0xefffefff; //8 bit data length USART1_CR3 = 0x00002000; //DMA disable USART1_BRR = 0x000001a1; //115200 // USART1_CR1 |= 0x00000008; //TX enabled USART1_CR1 = USART1_CR1 | 0x00000008; //TX enabled // USART1_CR1 |= 0x00000004; //RX enabled //USART1_TX on PC14 // PORTC_MODER &= 0xefffffff; //set PC14 as alternate function PORTC_MODER = PORTC_MODER & 0xefffffff; //set PC14 as alternate function // PORTC_AFRH &= 0xf0ffffff; //set PC14 as TxD function PORTC_AFRH = PORTC_AFRH & 0xf0ffffff; //set PC14 as TxD function // PORTC_OTYPER &= 0xffffbfff; //PC14 PP mode PORTC_OTYPER = PORTC_OTYPER & 0xffffbfff; //PC14 PP mode


Then I tryed to set another port on TxD, PB6 writing relative register and so at the pin I can see the the frame.
Mistery.

//USART1_TX on PB6 // PORTB_MODER &= 0xffffefff; //set PB6 as alternate function PORTB_MODER = PORTB_MODER & 0xffffefff; //set PB6 as alternate function // PORTB_AFRL &= 0xf0ffffff; //set PB6 as TxD function PORTB_AFRL = PORTB_AFRL & 0xf0ffffff; //set PB6 as TxD function // PORTB_OTYPER &= 0xffffffbf; //PB6 PP mode PORTB_OTYPER = PORTB_OTYPER & 0xffffffbf; //PB6 PP mode*/


Now I arrange my project to redirect the new pins.
I have another different question about the name of interrupt handle procedure. I can ask here or I have to open anoter post.
Thank you for your patience.
Valter