2023-12-15 3:22 AM
Hi, I observed a limitation in the STM32H7 reference manual saying that
"The current version of the SDMMC supports only one SD/SDIO/e•MMC card at any one
time and a stack of e•MMC."
So my application requires to control two SDIO slaves from both SDIO interfaces of STM32H747 at the same time, Is this realizable?
2023-12-15 7:27 AM
Hello @Rekhas19
Indeed, SDMMC interface only supports one card at a time, meaning that a device can only read from or write to one card at a time.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-25 3:14 AM
Hi Belaid,
Thank you for replying to my query.
When i saw the HAL and LLs of STM32H7 , i could not find any reference to CMD5, CMD52 and CMD53,which are SDIO specific functions. Please excuse me, I am very new to SDIO protocol. Can you please point to any reference API or example for those commands?
2023-12-25 3:52 AM
Hi,
As I understand the manual, every sdmmc interface can use one card, so using both sdmmc can connect to two SD cards, one on each sdmmc interface.
You want to use fatfs - or what? So give them two different drive names, maybe 0 and 1 .
2023-12-25 6:44 AM
You can find SD Card Specific commands here.
I hope this helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.