cancel
Showing results for 
Search instead for 
Did you mean: 

Update on STM32 embedded target for MATLAB® and Simulink®???

JWest.17
Associate II

A previous post mentioned an update was coming first quarter 2019. I'm still only seeing version 4.4.2. This version is not compatible with Matlab/Simulink 2018B...and that's a significant bummer. Would ST kindly provide an update?

Kind regards.

4 REPLIES 4

Hi,

​Please take into account the attached file to solve R2018b "invalid index" issue.

Best regards

Pascal

JWest.17
Associate II

Thank you, Sir! I will try that.

Kind regards,

Jeff

I'm still curious as to when an update to STM32 embedded target for MATLAB® and Simulink® will be out...presumably version 5.0.0?

Cyril FENARD
ST Employee

​Hi @JWest.17​ ,

The version 5.1.0 of STM32-MAT/TARGET has just been released at the end of July 2019.

Be aware that a lot of changes were involved in this release (in detail, alignment with STM32CubeMX version 5.1.0).

It is strongly recommended to upgrade to the most recent version of STM32-MAT/TARGET.

Regards.

Cyril