2018-02-02 01:11 AM
Hello everyone, i guess this is not the right place to ask, but official Atollic TrueSTUDIO forum gave me no answers. Maybe someone here had same problem as me.
Yesterday i moved from Keil to TrueSTUDIO IDE since it is free for STM32. After base code generation using STM32CubeMX i can't get over the error after building Debug. It does not find reference to any HAL and FreeRTOS functions. If i try to build Release the errors does not appear. Also then i try to RUN my project i get 'The selection cannot be launched, and there are no recent launches.'. What could be wrong?
P.S I am junior developer and never used debugging tools. Does Debug build and run is just as same as flash + use of debug tools?
Solved! Go to Solution.
2018-03-20 09:36 AM
Hello
matiukas.arnas
,
This issue is now fixed in the current CubeMX release.
Please, upgrade with CubeMX4.25 if not already done.
BR. Jeanne
2018-02-14 05:32 AM
Hello
matiukas.arnas
,This is a known bug reported in this
https://community.st.com/0D50X00009XkWopSAF
and will be fixed in coming version of CubeMx.Best Regards
Imen
2018-03-20 09:36 AM
Hello
matiukas.arnas
,
This issue is now fixed in the current CubeMX release.
Please, upgrade with CubeMX4.25 if not already done.
BR. Jeanne