cancel
Showing results for 
Search instead for 
Did you mean: 

Undefined reference to HAL & The selection cannot be launched

Arnas Matiukas
Associate II
Posted on February 02, 2018 at 10:11

Hello everyone, i guess this is not the right place to ask, but official Atollic TrueSTUDIO forum gave me no answers. Maybe someone here had same problem as me. 

Yesterday i moved from Keil to TrueSTUDIO IDE since it is free for STM32. After base code generation using STM32CubeMX i can't get over the error after building Debug. It does not find reference to any HAL and FreeRTOS functions. If i try to build Release the errors does not appear. Also then i try to RUN my project i get 'The selection cannot be launched, and there are no recent launches.'. What could be wrong?

P.S I am junior developer and never used debugging tools. Does Debug build and run is just as same as flash + use of debug tools

?

1 ACCEPTED SOLUTION

Accepted Solutions
Jeanne Joly
Senior III
Posted on March 20, 2018 at 17:36

Hello

matiukas.arnas

,

This issue is now fixed in the current CubeMX release.

Please, upgrade with CubeMX4.25 if not already done.

BR. Jeanne

View solution in original post

2 REPLIES 2
Imen.D
ST Employee
Posted on February 14, 2018 at 14:32

Hello

matiukas.arnas

,

This is a known bug reported in this

https://community.st.com/0D50X00009XkWopSAF

and will be fixed in coming version of CubeMx.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Jeanne Joly
Senior III
Posted on March 20, 2018 at 17:36

Hello

matiukas.arnas

,

This issue is now fixed in the current CubeMX release.

Please, upgrade with CubeMX4.25 if not already done.

BR. Jeanne