2019-03-29 3:29 AM
Hi,
I'm using STM32L0 series and working on UART to communicate with other module and I had chosen the polling method because i know the device max response time and exact data what i'm going to receive. I was running my application for testing and it worked fine for 24 hours and then after and MCU not able to receive data even the module is responding i don't understand this scenario, can anyone please suggest what could be the problem. Thanks in advance.
Regards,
Vijay Rakesh
HAL_UART_Transmit(&huart1,A_Buff,7,200);
HAL_UART_Receive(&huart1,Rx_Buf,4,5000); // Timeout value is 5 seconds to receive data
Solved! Go to Solution.
2019-04-01 8:10 AM
In my work I generally use a pair of FIFO buffers, and manage the reception/transmission from those directly in the IRQ Handler. The data is inserted and removed from the FIFO in a worker or foreground task so the interrupt is not loaded with processing overhead.
2019-03-29 5:23 AM
It is looking for trouble to process rx in polling. At least get a cyclic dma buffer in reception si there won t be any timeout issue.
2019-03-29 5:40 AM
Hi @S.Ma
Thanks for the reply, I don't have any idea on implementing DMA could please refer any document so that i can implement your suggestion and just now I have implemented UART interrupt method could this method can solve the above issue?
Regards,
Vijay Rakesh.
2019-03-29 5:54 AM
Check on stm32 library folders, nucleo board, usart projects.
2019-03-29 8:01 AM
They way you've implemented this with blocking functions is not conducive to concurrent transmit/receive. The HAL libraries just make such a mess of this rather than implementing some clean ring buffering.
My guess would be that you are getting over/under run type errors, or noise errors that don't get cleared and result in data loss. Compounded by fixed expectations about how much data will be received.
2019-03-31 10:17 PM
Hi @Community member ,
Thanks for the reply, what can be the best solution for implementing concurrent transmit/receive.
Regards,
Vijay Rakesh
2019-04-01 8:10 AM
In my work I generally use a pair of FIFO buffers, and manage the reception/transmission from those directly in the IRQ Handler. The data is inserted and removed from the FIFO in a worker or foreground task so the interrupt is not loaded with processing overhead.
2019-04-01 10:57 PM
I was actually trying to do the same after facing the issue but i couldn't find the call back for each UART data I receive and I can only find HAL_UART_RxCpltCallback() where I need to mention how much data I'm about to receive.
2019-04-01 11:53 PM
HAL functions are built for expected length messages. Otherwise, use length of "1".
Otherwise use LL (low layer) especially for USART peripheral as it's pretty manageable.