cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to Connect to Target STM32F412CEU6

caneralp
Associate

Hi. I have a simple custom board with STM32F412CEU6. I can't connect to the MCU using the ST-LINK through SWD.
 Here is the circuit. 

caneralp_0-1735815573795.png

I have tried different settings, still getting the error. 

caneralp_1-1735815601287.png

I verified all the voltages and settings. They all seem ok. 

I also measured the signals on SWD. 

caneralp_2-1735815665258.png

The only thing is the voltage level on SWD for the 0-V level looks suspicious. 

Can anyone help me to find the issue? 

Regards,
Caner 
Alp Electronix

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Thanks for the suggestions. 

 

1- There is a 4.7uF cap.

 

 

I just found the issue. I connected the VDD of the debugger pin to the same voltage of the board, now I can connect to the target. 

 

Regards,

Caner  

View solution in original post

2 REPLIES 2
mƎALLEm
ST Employee

Hello @caneralp and welcome to the community,

What is the value of the capacitor connected to VCAP pin?

According to the AN4488 "Getting started with STM32F4xxxx MCU hardware development":

SofLit_0-1735816599214.png

1- You need a 4.7uF capacitor on VCAP1 pin.

2- And a 4.7uF as decoupling capacitor connected to VDD not 2.2uF.

PS:

1- No need for NRST pullup resistor, as there is one internal in the chip.

2- Please use STM32CubeProgrammer to connect to the MCU instead of STLINK utility as it's a deprecated tool.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thanks for the suggestions. 

 

1- There is a 4.7uF cap.

 

 

I just found the issue. I connected the VDD of the debugger pin to the same voltage of the board, now I can connect to the target. 

 

Regards,

Caner