2018-11-19 05:40 PM
Hi
I am trying to install STM32CubeProgrammer on Ubuntu 18.04.1 LTS.
It apparently installs OK and places an icon on the desktop. When I start the app., a dialog with
"You are using OpenJDK, please Install OpenJFX
Debian: sudo apt-get install openjfx
or install Oracle JRE"
I have tried running "sudo apt-get install openjfx" but the problem still persists.
java is apparently installed
java --version
openjdk 10.0.2 2018-07-17
OpenJDK Runtime Environment (build 10.0.2+13-Ubuntu-1ubuntu0.18.04.3)
OpenJDK 64-Bit Server VM (build 10.0.2+13-Ubuntu-1ubuntu0.18.04.3, mixed mode)
could some one please help?
thanks
James
Solved! Go to Solution.
2018-11-19 11:02 PM
Ubuntu's OpenJFX is tied with OpenJDK 8.
You have two options:
2018-11-19 11:02 PM
Ubuntu's OpenJFX is tied with OpenJDK 8.
You have two options:
2018-11-20 02:23 AM
thanks "After Forever", I tried option 1 and selected the option to set to "/usr/lib/jvm/java-8-openjdk-amd64/jre/bin/java" which allowed the app to start.
cheers
James
2019-05-23 10:12 AM
Adopting your option, i get this message(with openjfx installed):
$ ./STM32CubeProgrammerLauncher
./STM32CubeProgrammerLauncher
/home/beantowel/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin
JavaFX NOT installed => warn user
Exception in thread "main" java.awt.AWTError: Assistive Technology not found: org.GNOME.Accessibility.AtkWrapper
at java.awt.Toolkit.loadAssistiveTechnologies(Toolkit.java:807)
at java.awt.Toolkit.getDefaultToolkit(Toolkit.java:886)
at java.awt.Window.getToolkit(Window.java:1358)
at java.awt.Window.init(Window.java:506)
at java.awt.Window.<init>(Window.java:537)
at java.awt.Frame.<init>(Frame.java:420)
at javax.swing.JFrame.<init>(JFrame.java:233)
2019-09-03 12:03 PM
@beantowel FWIW I was able to work around this problem on Debian by using Oracle's official JRE. https://www.java.com/en/download/linux_manual.jsp + https://github.com/chrishantha/install-java
2019-09-16 07:39 AM
My JAVA_HOME default to OpenJDK for coding Android applications to avoid all the legal stuff Oracle is throwing upon the community making everyone (including corporate management) scared of licens fees they "might" have to pay when one does not understand or TL;DR all the "small letters" . Since java fee may apply to embedded systems, it might be good if STM would switch to support OpenJDK (or another way to elminate this anxiety). I installed OpenJFX but that did not help. (Applies to Orcale's java it seems))
In my case no JAVA_HOME was set in any of my profile, nor the path to it. IThe reason was that something had sets some symbolic links :
command -v java
/usr/bin/java
ls -l /usr/bin/java
lrwxrwxrwx 1 root root 22 Jan 6 2018 /usr/bin/java -> /etc/alternatives/java
ls -l /etc/alternatives/java
lrwxrwxrwx 1 root root 43 Sep 16 21:47 /etc/alternatives/java -> /usr/lib/jvm/java-11-openjdk-amd64/bin/java
To switch to the JRE following I did
sudo update-alternatives --config java
Selection Path Priority Status
------------------------------------------------------------
* 0 /usr/lib/jvm/java-11-openjdk-amd64/bin/java 1101 auto mode
1 /usr/lib/jvm/java-11-openjdk-amd64/bin/java 1101 manual mode
2 /usr/lib/jvm/java-8-openjdk-amd64/jre/bin/java 1081 manual mode
3 /usr/lib/jvm/java-8-oracle/jre/bin/java 1081 manual mode
<Select 3>
source ~/.profile
sudo update-alternatives --config java
Selection Path Priority Status
------------------------------------------------------------
0 /usr/lib/jvm/java-11-openjdk-amd64/bin/java 1101 auto mode
1 /usr/lib/jvm/java-11-openjdk-amd64/bin/java 1101 manual mode
2 /usr/lib/jvm/java-8-openjdk-amd64/jre/bin/java 1081 manual mode
* 3 /usr/lib/jvm/java-8-oracle/jre/bin/java 1081 manual mode
The JAVA_HOME variable was not set accordingly to the jre as well.
Now run /STM32CubeProgrammer or STMCubeprogrammerIDE
et voila ! Love...
Plug in the STLINK and .. too much love..