cancel
Showing results for 
Search instead for 
Did you mean: 

UARTs Not Working On HSE Clock

JThom.15
Associate III

Hi ,

I am using an STM32F205 for my project. We were using HSI as the clock source before and found out that HSI will not work very well with high temperatures for UARTs, So we added an External crystal clock (16Mhz) but I am unable to get Comms out of UARTs now (There are some random values coming through uart sometimes). This is my clock config

RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLM = 14; RCC_OscInitStruct.PLL.PLLN = 240; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 4; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK) { Error_Handler(); } /** Enables the Clock Security System */ HAL_RCC_EnableCSS(); HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
View more

I also updated the HSE value in stm32f2xx_hal_conf.h to 16Mhz.

I am using platformIO as the IDE for this project.
Am I missing any configuration?

23 REPLIES 23
JThom.15
Associate III

Hi,

 

This is my USART1 () and RCC regsiters

with HSI 

JThom15_1-1708905538030.png

JThom15_2-1708905602191.png

With HSE

JThom15_4-1708905882871.png

 

JThom15_3-1708905816549.png

 

 

My five cents:

When you change from HSI to HSE (with a 16 MHz OSN/XTAL) - you cannot have the same PPL settings:

If HSI was based on 48 MHz (a guess) and you change to HSE with 16 MHz - the PLL config should look different, esp. to get the UART peripheral core clock as before,
If you make sure the PLL config results in the same UART peripheral clock - it should work.

But HSI on STM32F205 is 16MHz the same frequency as the external clock that I am using

Also I found out that, If I comment out HAL_RCC_ClockConfig(), the UARTS work fine. 

This is the order that I initialize the peripherals 

   

 

HAL_Init(); SystemClock_Config(); MX_I2C2_Init(); MX_I2C1_Init(); MX_I2C3_Init(); MX_UART_Init(); MX_ADC1_Init(); MX_GPIO_Init(); MX_CAN1_Init(); MX_CAN2_Init();

 

> This is my USART1 () and RCC regsiters

I meant, in RCC all registers which determine APB clock (i.e. besides RCC_CR also RCC_PLLCFGR and RCC_CFGR); and in UART registers which determine its baudrate and general working setup (UART_BRR, UART_CR1, UART_CR2).

My intention was to show you a way how *you* can find out, what's wrong, at the register level (which is how the microcontroller really works), and then work back into Cube/HAL to find out, where is the root of the problem - is it RCC/PLL setup, is it some other RCC setting, is it UART baudrate setup (and within that, is it a problem with the convoluted way how Cube/HAL determines the APB frequency from which UART's clock is derived), is it other UART setting, etc.

In other words, check everything impacting the baudrate, which is probably different from the expectation. You can confirm this by observing UART_Tx pin by oscilloscope/logic analyzer.

JW

Thanks JW,

I found its the UART->BRR register that changes when I use the HSE Clock. 

On HSI (16MHZ) the UART->BRR is 0x186a. But on HSE(16Mhz) UART->BRR changes to 0x2626.

If I manually update the BRR register (On HSE) with 0x186a then uart works fine at 9600 baudrate. 

Can anyone please explain why the BRR register changes If I use HSE with same clock frequency and  clock config as the HSI?

JThom.15
Associate III

I was able to set the MCO from HSE and it measures 16MHZ 

JThom15_0-1708994051292.png

So I am not sure why the UART baudrate changes when I use the HSE clock source

 

printf("%u\n", HSE_VALUE); printf("\n\nCore=%d, %d MHz\n", SystemCoreClock, SystemCoreClock / 1000000); { uint32_t clk; clk = HAL_RCC_GetHCLKFreq(); printf("HCLK=%9d, %6.2lf MHz\n", clk, (double)clk*1e-6); clk = HAL_RCC_GetPCLK1Freq(); printf("APB1=%9d, %6.2lf MHz\n", clk, (double)clk*1e-6); clk = HAL_RCC_GetPCLK2Freq(); printf("APB2=%9d, %6.2lf MHz\n", clk, (double)clk*1e-6); }

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Finally I found the issue,

We Copied stm32f2xx_hal_conf.h from PlatformIO Library in to our project. And changed the HSE_VALUE in the copied file. But the code was still using the stm32f2xx_hal_conf.h from the PlatformIO library which has got HSE_VALUE 25Mhz.

Thanks all for the Help

 

Great! Well done!

So, the clock config was wrong. Obvious. Smart, that you have found the root cause.

Yes, if one clock reference is wrong - the UART BRR has to be different (compared to what is expected to set).
Clock config can be very "tricky".

Enjoy your project now...