cancel
Showing results for 
Search instead for 
Did you mean: 

UART1 issue with STM32F303

ASaxe
Associate II

Hi All,

I am trying to receive data on USART1 but I am not getting data on USART1. Apart from USART1 USART2 & 3 is working fine.

As per datasheet USART1 pins are showing on (PE1, PE0 or PC5 & PC4). When I am use PE1 & PE0 that time USART1 is not working but if I config PC5 & PC4 pins USART1 working fine.

I want to know why this is happening because GND pins and RX TX pins are connected right and checked twice.

if anyone has any Idea let me know.

MCU : STM32F303CVT6 (Discovery board)

Data : on Terminal

/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart1;
 
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint8_t rx[6] = {'A','M','B','U','J'}, tx[6];
/* USER CODE END 0 */
 
/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
  
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART1_UART_Init();
  /* USER CODE BEGIN 2 */
 
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
		HAL_UART_Receive(&huart1, tx, 1, 10);
		if (tx[0] == 's'){
			HAL_UART_Transmit(&huart1, rx, sizeof(rx), 100);
			tx[0] = '0';
		}
  }
  /* USER CODE END 3 */
}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

> When I am use PE1 & PE0 that time USART1 is not working

Isn't there something else connected to some of these pins on the Discovery board? Check the schematics.

JW

ASaxe
Associate II

>> Isn't there something else connected to some of these pins on the Discovery board? Check the schematics.

No there is not any thing connected to the these pins on discovery schematic.