cancel
Showing results for 
Search instead for 
Did you mean: 

uart request response just during debug and debugger connected

carleslsregner
Associate III

Hello people,

I have been developing a firmware to be used in the stm32g051. One of the features is the ability to respon to request to get information from the uC. I used dma for the uart1 tx and rx.  I was happily developing and testing the new feature added into the stm32g051. Then when I use it without the debugger, it is unable to stablish communications between the PC and the microcontroller. 

The curious thing is the fact that I remove the debugger -I disconnect it- and the communication still works. It is the "reset" without debugger what is unable to stablish the connection.  

I change the clocks following the several  post regarding this problem but the solution still eludes me. 

 

 

 

10 REPLIES 10
TDK
Super User

If PVD is triggered but the interrupt isn't implemented anywhere, that would show up as a random call to Default_Handler, which may show up as WWDG_IRQHandler as shown.

 

Implementing the handler isn't going to solve your power problems, of course.

If you feel a post has answered your question, please click "Accept as Solution".