UART Data Getting DMA'd In Wrong Order After First Packet
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-24 8:28 AM
I have a device that receives six bytes via the UART. There is a known SOF and EOF byte. The first time I get the data, all is well. But subsequent receptions are "corrupted": either the EOF byte is first, or sometimes I get two SOF bytes in a row (and no EOF byte at all).
The DMA is set up for normal (non-circular) operation. Does anyone see why this would be happening? I only call the RX transfer after the callback has been run, so data still being transferred shouldn't be an issue.
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_USART2_UART_Init();
MX_LPUART1_UART_Init();
/* Infinite loop */
while (1)
{
switch(state)
{
case STATE_READY_TO_RECEIVE:
Result = HAL_UART_Receive_DMA (&huart2, RX_Data, 6);
// check result for errors
break;
case STATE_READY_TO_SEND:
Result = HAL_UART_Transmit_DMA(&hlpuart1, ACK_Data, 3);
// check result for errors
state = STATE_SENDING;
break;
case STATE_RECEIVING:
case STATE_SENDING:
// Nothing to do, waiting for the hardware
break;
default:
// handle bad state error
break;
}
}
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if(RX_Data[0] == 0xA1)
{
state = STATE_READY_TO_SEND;
}
else
{
memset(RX_Data, 0, 6);
}
//Process data
}
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
if (state == STATE_SENDING)
{
state = STATE_READY_TO_RECEIVE;
}
else
{
// error - state machine broken
}
}
- Labels:
-
DMA
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-24 9:11 AM
If you're dealing with multiple bytes you need to be dealing with the potential for bytes lost in reception, or synchronization issues.
The DMA/IT forms don't handle/manage timeout situations well.
On most STM32 there's an interrupt per-byte on UARTs, make something that manages this in a stateful manner. If the HAL doesn't suit this well, you're not obliged to use it.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-25 12:27 AM
Hi @Community member​
Some questions to be sure to understand your use case :
- what happens if some bytes are received during the transmit of Ack message ? I guess they will fill reception register and could lead to have overrun flag raised.
- If Fifo are available on your STM32, are you using Tx and/or Rx FIFO ? this could help to reduce cases of overrun if Rx Fifo is enabled.
- How is declared your "state" variable ? as addressed from IRQ routine and from main program, depending on compiler optimizations options, please make sure it is declared as "volatile" (or __IO).
Regards