cancel
Showing results for 
Search instead for 
Did you mean: 

TrueSTUDIO run configuration

Krystof Vanek
Associate II
Posted on March 07, 2018 at 12:44

Hello,

is there a way to create run configuration in TrueSTUDIO in a same way as it is in SW4STM32?

I would like to 'launch' the code without entering the debug perspective. Just flash and run.

Thanks for helping.

#truestudio
16 REPLIES 16
Posted on March 08, 2018 at 12:16

try st-link to see if you get the same...

64-bit Linux Fedora here, no terminal problems with texane tool...

Posted on March 08, 2018 at 12:47

My system might be funky

I'm on Arch and I've tried both texane version (installed through AUR) and community repository version through pacman. They both giving kinda strange output. At first sight one can be scared, however nothing bad is really written there. Its just red

0690X0000060A18QAE.png

Do you have similar behavior?

Posted on March 09, 2018 at 06:02

Please help me with TrueStudio configuration with STM32L475 board.

Becuase in the hands-on or getting started only mention IAR (EWARM).

Thank you very much in advance.

Suryadi

Posted on March 09, 2018 at 07:47

No, no problems in displaying colored text on a terminal...

Try to install colorgcc and rxvt-unicode-256color and see if it makes any difference...

Posted on March 09, 2018 at 07:52

- which version of TrueStudio?

- what kind of board?

- what API are you using in development (SPL, HAL, LL)?

Posted on April 26, 2018 at 09:15

Hello, I tried to set up this configuration in my TrueStudio, but there is always an error.

0690X00000604byQAA.jpg

My configuration is :

0690X00000604c3QAA.jpg

Can you help me solve it? Thank you.

Posted on April 26, 2018 at 13:43

Hi,

I have noticed that your working directory is not like mine. I'm not sure if it can be an error or not.

Otherwise, I've issues if I do not explicitely select the project in the project explorer before launching the external tool. Check that the project you want to flash is selected before trying to run the external tool.

Have a nice day.