cancel
Showing results for 
Search instead for 
Did you mean: 

TrueStudio does not build the imported example for BlueNRG-2

idolezal
Associate II

I imported the BLE Beacon example from

C:\ST\BlueNRG-1_2 DK 3.2.2\Project\BLE_Examples\BLE_Beacon\WiSE-Studio\STEVAL-IDB008V1M

in Atollic TrueStudio 9.3.0 ("Existing Projects into Workspace")

but after clicking the 'Build' button, the console prints:

**** Build of configuration Release for project BLE_Beacon ****

Nothing to build for project BLE_Beacon

There is a folder c:\Data\ARM\BLE_Beacon in my workspace, but it contains only

.cproject

.project

BlueNRG2.ld

files.

Any advice?

2 REPLIES 2

Is that example supposed to work with TrueStudio?

Note that TrueStudio is Not Recommended for New Designs (NRND) - STM32CubeIDE is the replacement: 

0693W00000QLuICQA1.png 

although there's some tips from @Nikita91​  on "upgrading" TrueStudio in this thread:

https://community.st.com/s/question/0D73W000001P21ASAS/detail?s1oid=00Db0000000YtG6&s1nid=0DB0X000000DYbd&emkind=chatterCommentNotification&s1uid=0050X000007vvPr&emtm=1658490328919&fromEmail=1&s1ext=0

idolezal
Associate II

Both STM32CubeIDE and STM32CubeMX do not support BlueNRG, as given in some threads here. They do not offer BlueNRG-2 in MCU selection.