cancel
Showing results for 
Search instead for 
Did you mean: 

Trigger the OnePulseMode by software

Lecordier.Guy
Associate III
Posted on April 04, 2016 at 13:37

Hello,

I want to use the OnePulseMode timer on software demand.

On the documentation and even in the HAL the triggering by software is not mentioned only by an external signal is mentioned.

I did some testing and by programming the CEN bit I get a Pulse.

So is there a reason to forbid the software triggering. I used the STM32F429.  

Regards

1 REPLY 1
Radosław
Senior II
Posted on April 04, 2016 at 13:50

>>So is there a reason to forbid the software triggering. I used the STM32F429.  

NO

If you stop timer before update, consider software update generation to reset timer.