2016-04-04 04:37 AM
Hello,
I want to use the OnePulseMode timer on software demand.
On the documentation and even in the HAL the triggering by software is not mentioned only by an external signal is mentioned. I did some testing and by programming the CEN bit I get a Pulse. So is there a reason to forbid the software triggering. I used the STM32F429.Regards
2016-04-04 04:50 AM
>>So is there a reason to forbid the software triggering. I used the STM32F429.
NO
If you stop timer before update, consider software update generation to reset timer.