cancel
Showing results for 
Search instead for 
Did you mean: 

Trainings in 2015 in Europe, January to June (v1.3)

Tomas DRESLER
Senior II
Posted on January 06, 2015 at 19:23

Dear colleagues and partners,

here I am attaching the plan for ST public trainings. They are typically 3-day long with detailed core and peripheral usage and hands-on.

If you're interested, please let me know at microsupport.europe -at- st.com and me or my colleagues will reply with full catalogue or details on selected course. Same address is available for registration, too.

Best regards,

Tomas

January

February

March

April

May

June

STM32F0

& F3

W20 Prague

STM32F334

W18 Milano

STM32

F4+emWin

W3 Prague

W14 Prague

 

(special guest I2ST

 

w. Java +1 day)

W27 Prague

STM32

L0

W6 Prague

Motor Control with ST

solutions

W4 Prague

W12 Stockholm

 

W18 Munich

W24 Paris

Advanced C

W15 Munich

 

RTOS, USB, Ethernet, SSL

 

W26 Prague

#stm32
10 REPLIES 10
lowpowermcu
Associate II
Posted on January 29, 2015 at 17:24

Hi Edison,

Good news !

It it a free training ? 

If no how much does it cost ?

Regards

Tomas DRESLER
Senior II
Posted on February 05, 2015 at 17:25

Hi lowpowermcu,

the trainings are free of charge, ST lunch included :)

Edison_CZ

giuseppe239955_st
Associate II
Posted on March 25, 2015 at 11:52

Thank you for the information.

Any chance to get a more general training event on STM32 (not specifically F334) soon in Italy?

Posted on May 22, 2015 at 21:33

Was starting to wonder if the STM32F7 had fallen off the road map.

http://www.st.com/web/en/seminar/stm32f7-hands-on-seminars

Not seeing anything in the North-American market, and had an ATSAMV71-XULT for several weeks.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 27, 2015 at 23:51

> Not seeing anything in the North-American market

An excuse for a trip over here? We could sample a couple of historical pubs in Prague... :)

JW

qwer.asdf
Senior
Posted on June 01, 2015 at 14:21

> Was starting to wonder if the STM32F7 had fallen off the road map.

Well all the documentation (datasheets, reference manuals, etc.) seem to be ready (except the HAL documentation), there's even a more than 20-page errata already, and the Cube for STM32F7 is also ready, and there are two evaluation boards (STM32746G-EVAL and STM32756G-EVAL) out there that you can get now, so I think it must be in the final stages.
Posted on June 01, 2015 at 16:21

I guess my frustration is the paper launch of the ''first m7'' from late

http://www.st.com/web/en/press/p3606s

, and we're in late May 2015 (very late today). When I get some ST silicon, I'll bench it against the Atmel part, which has been in retail channels for +6 weeks.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
piyush2
Associate II
Posted on June 25, 2015 at 17:49

Hey guys can you put the video and other tutorials of the seminar if they are available.

Regards

piyush2
Associate II
Posted on June 25, 2015 at 17:52

if possible can you post the munich Advanced C seminar video and tutorials or documents