cancel
Showing results for 
Search instead for 
Did you mean: 

TOO Many loads!!!

Ala
Senior
 
This discussion is locked. Please start a new topic to ask your question.
19 REPLIES 19
T J
Lead

did you initialise those pins at startup ? you would have to set the alternate function to GPIO.

did you use the cube ?

S.Ma
Principal

how did you define the port pins? Push pull, internal pull-up, etc... there the pin configuration is missing.

T J
Lead

not using the cube ?

Dear T J

yes I did initialized them completely, otherwise it wouldn't work at all.

and yes I used the cube, is it wrong?

yes I didn't bring them up here as it would made my code hard to understand, so I just mentioned the relevant parts.

if you want to send the cube file over, we will look a it..

why didnt you name the pins? so much easier to follow.

Dear T J

here is the cube... hope you can guide me through..

Looks like you are running at 12MHz, which is very slow...

Do you have a 25MHz crystal on the PCB ?

are you sure its running at 25MHz ? do you have a scope for that ?

is this PCB hand soldered ?

did you want to send your code ?

there is no PCB yet, but there will be, I can send you the code but how does the 12MHz slow clock have anything to do with turning on the heat elements?