2023-12-06 2:43 AM
Hello Everyone
i am using stm32G031J6 Microcontroller. I want to generate a PWM signal from Timer 1 working as slave in gated mode, that has a pulse width = 10us and pulse period = 44us In this microcontroller i am using Timer 3 as a Master which has a PWM signal that has a Burst width = 7ms and Burst Period = 16.67 ms. Currently i am getting PWM signal on my Timer 1 and timer 3, but the problem is that They are Not SYNCHRONISED, can anyone help me please
This is my configuration for Timer 3 as Master in Cube MX , slave mode - Disable, Trigger source - Internal clock, Channel3 - PWM Generation No output, Parameter settings: Prescaler - 64-1, Counter Period - 16676-1, PWM Generation channel 3 - PWM mode 2 and Pulse : 7000-1
This is my configuration for Timer 1 as a slave in gated mode, channel - PWM Generation CH1, Trigger Source:ITR2
Parameter settings : Prescaler : 64-1, Counter Period: 44-1, Pulse : 10
Can anyone please help how i can synchronise these two timers
Solved! Go to Solution.
2023-12-07 8:27 AM
Hii
Thanks for your quick response. Yes this is exactly what PWM signal do. The PWM signal which i am getting is Jumping and they are not periodic in nature, they are changing their state frequently.
Second Answer : I want TIM1_CH1 to be a slave and only output during the high period of TIM3_CH3. So when TIM3_CH3 is High we get pwm output from TIM1_CH1 and when TIM_CH3 is low we do not want any PWM from TIM_CH1.
Something like this: Please go to Periodic Trigger signal
2023-12-07 9:02 AM
Read out and post content of TIM registers.
JW