2020-08-24 5:04 AM
The STM32G4 series offers dithering to enhance the PWM ratio. My question is, if dithering can be used on ALL the compare channels of the same timer?
Specifically, we generate a center-aligned PWM with two output compare channels 180° shifted. CCR1 and CCR2 are changed simultaneously to change both duty cycle. Can dithering be applied to both registers?
2020-08-24 5:43 AM
> The STM32G4 series offers dithering to enhance the PWM ratio.
That's no 'G4-specific feature, it's just software regularly changing the duty cycle.
Okay so hardware dithering is a new feature in G4 timers.
> Can dithering be applied to both registers?
As dithering is nothing more than changing duty cycle, so... why not?
According to RM, yes; you can't avoid it working on all CCRx registers.
JW