cancel
Showing results for 
Search instead for 
Did you mean: 

Timer Configuration for specific duration

dbgarasiya
Senior II

Hello ,

I want to configure a timer which start and runs for specific duration and stops automatically

and when again i want to start that timer i could be able to start timer and agian stops automatically

duration is fixed all time

Dipak Garasiya

This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
berendi
Principal

Enable the timer in RCC. This is dependent on the MCU series, check the reference manual to see which register in RCC has the APB enable bit for the timer.

Set the prescaler (if needed) in PSC, and set the UG bit in EGR.

TIMx->PSC = prescaler - 1; TIMx->EGR = TIM_EGR_UG;

Set the auto reload register (ARR) to the required timer period - 1

TIMx->ARR = period - 1;

Start the timer by setting the counter enable (CEN) and one pulse mode (OPM) bits in CR1.

TIMx->CR1 = TIM_CR1_CEN|TIM_CR1_OPM;

If the timer period is elapsed, (TIMx->CR1 & TIM_CR1_CEN) will be automatically cleared, the timer stops, and you can repeat the line above to start it again.

dbgarasiya
Senior II

If I want to set timer of 5 sec , how to calculate prescaler and period

my system clock is 16MHZ

You need the peripheral clock frequency of the timer, not the system clock. You have already found out in the previous step which APB bus the timer is connected to, so note the frequency of that APB bus.

The frequency is the number of cycles in one second. For a timeout of 5 seconds, the required number of cycles is five times the frequency.

Most timers have 16 bit counters (check the timer main features in the reference manual), and the required number of cycles is likely greater than 2^16, so you have to factorize it into a product of two numbers, both less than 2^16. Then use one of them as the prescaler, the other one as the period.

dbgarasiya
Senior II

Thanks @berendi​ 

I have tried your code but i am not getting clearing register. like i am posting my code with this post

i have test to set pin high for some time to test using timer

RCC->APB1ENR |= (1<<1); // Enable clock for TIM3

TIM3->PSC = 999;    // Int clk divided by 1000(999+1)

TIM3->EGR = TIM_EGR_UG; // Forcing to generate a update

TIM3->ARR = 7999; // Counts from 0 to 7999

TIM3->CR1 = TIM_CR1_CEN|TIM_CR1_OPM;

while ( (TIM3->CR1 & TIM_CR1_CEN) != 0)

{

HAL_GPIO_WritePin(GPIOH, GPIO_PIN_6,GPIO_PIN_SET);

}

Best Regards

Dipak Garasiya

How do you know that CEN does not get cleared? What do TIM3 registers contain when you let it run for a while and stop it? Does it exit the loop?

dbgarasiya
Senior II

I have checked by debugging code , while loop never exits. and stops code there

i have attached my debugging sceenshot where you will get TIM3 register value at timer of entering while loop

Best Regards

Dipak Garasiya

I can't see the screenshot.

Check the timer registers. Do PSC, ARR and CR1 contain the values you've set? Is the counter changing?

waclawek.jan
Super User

What's *after* the while loop?

Put some code there, e.g. another write to a GPIO pin.

JW

dbgarasiya
Senior II

Sorr for inconvience , i have just attached sceenshot with this post