2023-09-10 6:44 PM
Hi everyone, I meet a problem and I'm not sure it's MCU issue or I program not proper.
I meet this issue both on the STM8 and STM32 MCUs.
I enable TIM_2 Ch1 as input to capture the signal and TIM_2 Ch2 as output to do the compare function.
void init_TIM_2
{
RCC.APB1ENR.bit.TIM2EN = 1;
..
TIM2.CCMR1.bit.Inmode.IC1S = 1;
TIM2.CCMR1.bit.Inmode.IC1PSC = 0;
TIM2.CCER.bit.CC1P = 0;
TIM2.CCER.bit.CC1E = 1;
..
TIM2.CCMR1.bit.Outmode.OC2S = 0;
TIM2.CCER.bit.CC2E = 1;
TIM2.DIER.bit.CC2IE = 1;
..
}
Also I enable the global interrupt with the NVIC module. So the interrupt is working.
And what I do in the interrupt just set a new compare value and toggle an GPIO pin.
void TIM2_ISR(void)
{
if (TIM2.SR.bit.CC2IF)
{
int p = TIM2_CCR;
int new_val = 0;
..
// Calculate a new compare value
// Toggle the GPIO pin
..
TIM2.CCR = p + new_val;
TIM2.SR.bit.CC2IF = 0;
}
}
I found it will miss the compare value sometime.
I trace the CCR value and timer counter value of TIM2, the CCR value should be greater than the counter value in normal case. But I found it's not triggered the ISR and the counter just exceed the CCR value sometimes.
If I program not proper, please have some advise for me. Thank you!
The actual data trace list as below:
| TIM2 CCR value | TIM2 counter value | Notes |
| 21735563 | 21729923 | |
| 21735563 | 21735024 | |
| 21735563 | 21740124 | The counter val > CCR and no interrupt event |
| 21735563 | 21745225 |
Solved! Go to Solution.
2023-09-12 11:30 PM
@waclawek.jan It really helps me a lot. I thought what I set is only 1 bit not a whole bits of register. But I trace the assembly code and it really did the LDR->BIC->STR and it cause the other interrupt flags clear either.
Many thanks.
2023-09-14 12:38 AM
The reasons why for register accesses the bit-fields are harmful and useless: