2024-05-30 07:33 AM - edited 2024-06-03 01:06 AM
EDIT* for those seeking a solution, JW in the replies below pointed out that the DIER register for TIM1 never enabled the interrupt bit for the commutation event and the mistake was that I used
HAL_TIMEx_ConfigCommutEvent(&htim1, TIM_TS_NONE, TIM_COMMUTATION_SOFTWARE);
Instead of
HAL_TIMEx_ConfigCommutEvent_IT(&htim1, TIM_TS_NONE, TIM_COMMUTATION_SOFTWARE);
---------------------------------------------------------------------------------------------------------------------------------------------------------
Dear whomever may read this,
I've been working with PWM on TIM1 with the NUCLEO-F429ZI, I have three channels and their complementary channels active. This is an iterative test project, where I am bring function to life one step at a time. The following is the configuration for TIM1 (Note channel 2, 2N and 3, 3N have the same configuration as 1 and 1N).
TIM1 Channel Modes
TIM1 Parameters
After being happy with the PWM timer, I enabled the commutation interrupt
TIM1 Interrupts
In the beginning I also had the update interrupt and that was working and firing. Then in my loop I was simply trying to fire a commutation generation event about once every second (just rough test). The if statement runs but the "void TIM1_TRG_COM_TIM11_IRQHandler(void)" routine never runs for some reason.
I then took the event generation out of the loop and did it once in the beginning made a test to see if the commutation flag is being set (it is), but it's never serviced and then cleared. So the LED kept toggling. It can be manually reset.
Here is the current version of my main, in the middle of trying out some tests. The code is temporary test code after trying to debug. But from all I can see I have configured the timer to accept the software events, I thought "void TIM1_TRG_COM_TIM11_IRQHandler(void)" would handle that. Perhaps I am wrong there.
int main(void)
{
HAL_Init();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_TIM1_Init();
MX_ADC1_Init();
MX_USART3_UART_Init();
/* Initialize interrupts */
MX_NVIC_Init();
HAL_TIM_Base_MspInit(&htim1);
HAL_TIMEx_ConfigCommutEvent(&htim1, TIM_TS_NONE, TIM_COMMUTATION_SOFTWARE);
// TODO: This is needed for the update event
HAL_TIM_Base_Start_IT(&htim1);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_2);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3);
HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_3);
HAL_ADC_Start(&hadc1);
uint16_t adc_val = 0;
float duty_cycle = 0.5f;
uint16_t period_pwm = __HAL_TIM_GET_AUTORELOAD(&htim1);
uint32_t last_event = HAL_GetTick();
const uint32_t tick_between = 1000;
HAL_TIM_GenerateEvent(&htim1, TIM_EVENTSOURCE_COM);
while (1)
{
HAL_ADC_PollForConversion(&hadc1, 1000);
adc_val = HAL_ADC_GetValue(&hadc1);
duty_cycle = adc_val / 4095.0f;
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_1, duty_cycle * period_pwm);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_2, 0.5 * duty_cycle * period_pwm);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_3, 0.25 * duty_cycle * period_pwm);
if ((HAL_GetTick() - last_event) > tick_between)
{
if (__HAL_TIM_GET_FLAG(&htim1, TIM_FLAG_COM))
{
HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
__HAL_TIM_CLEAR_FLAG(&htim1, TIM_FLAG_COM);
}
last_event = HAL_GetTick();
}
}
HAL_ADC_Stop(&hadc1);
}
I can send further information and answer question if anyone has any idea what is happening, I'm no HAL expert and this is a step in my learning journey. I'd appreciate the help.
Solved! Go to Solution.
2024-05-31 07:01 AM
In your timer screenshots, TIMx_DIER=0x1, i.e. only UIE is set, not the commutation interrupt enable bit.
I don't use Cube/HAL.
JW
2024-05-30 07:44 AM
I should perhaps add some of the following functions
static void MX_NVIC_Init(void)
{
/* TIM1_TRG_COM_TIM11_IRQn interrupt configuration */
HAL_NVIC_SetPriority(TIM1_TRG_COM_TIM11_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM1_TRG_COM_TIM11_IRQn);
}
Enabling the function that I thought would handle the Event Generation for TIM_EVENTSOURCE_COM
void HAL_TIMEx_CommutCallback(TIM_HandleTypeDef *htim)
{
char msg[30] = "Made it to the callback\r\n";
HAL_UART_Transmit(&huart3, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
}
Function meant originally to handle the commutation callback
void TIM1_TRG_COM_TIM11_IRQHandler(void)
{
/* USER CODE BEGIN TIM1_TRG_COM_TIM11_IRQn 0 */
char msg[30] = "Made it COM IRQ Handler\r\n";
HAL_UART_Transmit(&huart3, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
/* USER CODE END TIM1_TRG_COM_TIM11_IRQn 0 */
HAL_TIM_IRQHandler(&htim1);
/* USER CODE BEGIN TIM1_TRG_COM_TIM11_IRQn 1 */
/* USER CODE END TIM1_TRG_COM_TIM11_IRQn 1 */
}
I have verified UART working, I've also had LED toggling in there instead to no luck.
2024-05-30 09:55 AM
Cube/HAL is open source, so you can debug it as your own code.
If you've verified by reading the TIM registers that the commutation event happened (the respectrive flag in TIMx_SR is set) and the commutation interrupt is enabled (respective flag in TIMx_DIER), then the processor should fire the respective interrupt (as you've said, it should be TIM1_TRG_COM_TIM11_IRQHandler, but that depends on how exactly the vector table, usually in startup code, is constructed). So place a breakpoint there, and if the interrupt does fire and stops on that breakpoint, walk through Cube's code to see, why does it not vector to the your callback. If the interrupt does not fire, follow steps from here.
JW
2024-05-31 04:46 AM
Dear JW,
Thanks for the reply, I had tried some debugging yesterday. But I'm relatively new to HAL and interrupts especially, I've been trying to get a better hang of it and thought I understood the process more clearly.
I will detail here my debugging process, I would appreciate if someone more knowledgeable could point me to mistakes and next steps if any are available.
First thing I did was to also enable the update event for TIM1 to see if I could get any interrupt going and found for that that I needed the following line in the start. (Before I had only started the PWM channels).
HAL_TIM_Base_Start_IT(&htim1);
This managed to fire the following interrupt.
void TIM1_UP_TIM10_IRQHandler(void)
I've also checked the TIM1->SR and the COMIF bits, before and after event generation.
Before Event Generation
After Event Generation
After The Clear Flag
Satisfied that the COM interrupt flag is set and I can manually clear it I changed the main loop back to
HAL_TIM_GenerateEvent(&htim1, TIM_EVENTSOURCE_COM);
while (1)
{
HAL_ADC_PollForConversion(&hadc1, 1000);
adc_val = HAL_ADC_GetValue(&hadc1);
duty_cycle = adc_val / 4095.0f;
// Much better way to reconfigure the pulse duration
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_1, duty_cycle * period_pwm);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_2, 0.5 * duty_cycle * period_pwm);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_3, 0.25 * duty_cycle * period_pwm);
if ((HAL_GetTick() - last_event) > tick_between)
{
HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
last_event = HAL_GetTick();
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
So I generate the event and then go into the loop, the u
void TIM1_TRG_COM_TIM11_IRQHandler(void)
pdate event fires but never the
void TIM1_TRG_COM_TIM11_IRQHandler(void)
Perhaps then I'm configuring that interrupt wrong. In main before the look, AFTER MX_TIM1_Init(); I have
/* Initialize interrupts */
MX_NVIC_Init();
/* USER CODE BEGIN 2 */
HAL_TIMEx_ConfigCommutEvent(&htim1, TIM_TS_NONE, TIM_COMMUTATION_SOFTWARE);
Where MX_NVIC_Init() is as follows
static void MX_NVIC_Init(void)
{
/* TIM1_TRG_COM_TIM11_IRQn interrupt configuration */
HAL_NVIC_SetPriority(TIM1_TRG_COM_TIM11_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(TIM1_TRG_COM_TIM11_IRQn);
}
As I have said I'm not expert on HAL and I can have troubles, from what I know I think I'm doing things right. But I'd be very happy to learn what I'm doing wrong :)
p.s. I put a break point on the interrupt hander for TIM1_TRG_COM_TIM11_IRQHandler, it never runs.
2024-05-31 05:05 AM
I'd like to add the contents of the NVIC registers, I've been trying to read through RM0090 to find the ISRx registers but have not been able to locate that. Thus I have a hard time knowing whether the interrupt enable lines are actually configuring things correctly. I attach here a picture of the registers, If anyone knows what page in RM0090 it is or in some other document I'd appreciate that.
NVIC ISERx
I also attach here the vector table in the start up, line 50 below has the interrupt in question.
.section .isr_vector,"a",%progbits
.type g_pfnVectors, %object
g_pfnVectors:
.word _estack
.word Reset_Handler
.word NMI_Handler
.word HardFault_Handler
.word MemManage_Handler
.word BusFault_Handler
.word UsageFault_Handler
.word 0
.word 0
.word 0
.word 0
.word SVC_Handler
.word DebugMon_Handler
.word 0
.word PendSV_Handler
.word SysTick_Handler
/* External Interrupts */
.word WWDG_IRQHandler /* Window WatchDog */
.word PVD_IRQHandler /* PVD through EXTI Line detection */
.word TAMP_STAMP_IRQHandler /* Tamper and TimeStamps through the EXTI line */
.word RTC_WKUP_IRQHandler /* RTC Wakeup through the EXTI line */
.word FLASH_IRQHandler /* FLASH */
.word RCC_IRQHandler /* RCC */
.word EXTI0_IRQHandler /* EXTI Line0 */
.word EXTI1_IRQHandler /* EXTI Line1 */
.word EXTI2_IRQHandler /* EXTI Line2 */
.word EXTI3_IRQHandler /* EXTI Line3 */
.word EXTI4_IRQHandler /* EXTI Line4 */
.word DMA1_Stream0_IRQHandler /* DMA1 Stream 0 */
.word DMA1_Stream1_IRQHandler /* DMA1 Stream 1 */
.word DMA1_Stream2_IRQHandler /* DMA1 Stream 2 */
.word DMA1_Stream3_IRQHandler /* DMA1 Stream 3 */
.word DMA1_Stream4_IRQHandler /* DMA1 Stream 4 */
.word DMA1_Stream5_IRQHandler /* DMA1 Stream 5 */
.word DMA1_Stream6_IRQHandler /* DMA1 Stream 6 */
.word ADC_IRQHandler /* ADC1, ADC2 and ADC3s */
.word CAN1_TX_IRQHandler /* CAN1 TX */
.word CAN1_RX0_IRQHandler /* CAN1 RX0 */
.word CAN1_RX1_IRQHandler /* CAN1 RX1 */
.word CAN1_SCE_IRQHandler /* CAN1 SCE */
.word EXTI9_5_IRQHandler /* External Line[9:5]s */
.word TIM1_BRK_TIM9_IRQHandler /* TIM1 Break and TIM9 */
.word TIM1_UP_TIM10_IRQHandler /* TIM1 Update and TIM10 */
.word TIM1_TRG_COM_TIM11_IRQHandler /* TIM1 Trigger and Commutation and TIM11 */
.word TIM1_CC_IRQHandler /* TIM1 Capture Compare */
.word TIM2_IRQHandler /* TIM2 */
.word TIM3_IRQHandler /* TIM3 */
.word TIM4_IRQHandler /* TIM4 */
.word I2C1_EV_IRQHandler /* I2C1 Event */
.word I2C1_ER_IRQHandler /* I2C1 Error */
.word I2C2_EV_IRQHandler /* I2C2 Event */
.word I2C2_ER_IRQHandler /* I2C2 Error */
.word SPI1_IRQHandler /* SPI1 */
.word SPI2_IRQHandler /* SPI2 */
.word USART1_IRQHandler /* USART1 */
.word USART2_IRQHandler /* USART2 */
.word USART3_IRQHandler /* USART3 */
.word EXTI15_10_IRQHandler /* External Line[15:10]s */
.word RTC_Alarm_IRQHandler /* RTC Alarm (A and B) through EXTI Line */
.word OTG_FS_WKUP_IRQHandler /* USB OTG FS Wakeup through EXTI line */
.word TIM8_BRK_TIM12_IRQHandler /* TIM8 Break and TIM12 */
.word TIM8_UP_TIM13_IRQHandler /* TIM8 Update and TIM13 */
.word TIM8_TRG_COM_TIM14_IRQHandler /* TIM8 Trigger and Commutation and TIM14 */
.word TIM8_CC_IRQHandler /* TIM8 Capture Compare */
.word DMA1_Stream7_IRQHandler /* DMA1 Stream7 */
.word FMC_IRQHandler /* FMC */
.word SDIO_IRQHandler /* SDIO */
.word TIM5_IRQHandler /* TIM5 */
.word SPI3_IRQHandler /* SPI3 */
.word UART4_IRQHandler /* UART4 */
.word UART5_IRQHandler /* UART5 */
.word TIM6_DAC_IRQHandler /* TIM6 and DAC1&2 underrun errors */
.word TIM7_IRQHandler /* TIM7 */
.word DMA2_Stream0_IRQHandler /* DMA2 Stream 0 */
.word DMA2_Stream1_IRQHandler /* DMA2 Stream 1 */
.word DMA2_Stream2_IRQHandler /* DMA2 Stream 2 */
.word DMA2_Stream3_IRQHandler /* DMA2 Stream 3 */
.word DMA2_Stream4_IRQHandler /* DMA2 Stream 4 */
.word ETH_IRQHandler /* Ethernet */
.word ETH_WKUP_IRQHandler /* Ethernet Wakeup through EXTI line */
.word CAN2_TX_IRQHandler /* CAN2 TX */
.word CAN2_RX0_IRQHandler /* CAN2 RX0 */
.word CAN2_RX1_IRQHandler /* CAN2 RX1 */
.word CAN2_SCE_IRQHandler /* CAN2 SCE */
.word OTG_FS_IRQHandler /* USB OTG FS */
.word DMA2_Stream5_IRQHandler /* DMA2 Stream 5 */
.word DMA2_Stream6_IRQHandler /* DMA2 Stream 6 */
.word DMA2_Stream7_IRQHandler /* DMA2 Stream 7 */
.word USART6_IRQHandler /* USART6 */
.word I2C3_EV_IRQHandler /* I2C3 event */
.word I2C3_ER_IRQHandler /* I2C3 error */
.word OTG_HS_EP1_OUT_IRQHandler /* USB OTG HS End Point 1 Out */
.word OTG_HS_EP1_IN_IRQHandler /* USB OTG HS End Point 1 In */
.word OTG_HS_WKUP_IRQHandler /* USB OTG HS Wakeup through EXTI */
.word OTG_HS_IRQHandler /* USB OTG HS */
.word DCMI_IRQHandler /* DCMI */
.word 0 /* Reserved */
.word HASH_RNG_IRQHandler /* Hash and Rng */
.word FPU_IRQHandler /* FPU */
.word UART7_IRQHandler /* UART7 */
.word UART8_IRQHandler /* UART8 */
.word SPI4_IRQHandler /* SPI4 */
.word SPI5_IRQHandler /* SPI5 */
.word SPI6_IRQHandler /* SPI6 */
.word SAI1_IRQHandler /* SAI1 */
.word LTDC_IRQHandler /* LTDC_IRQHandler */
.word LTDC_ER_IRQHandler /* LTDC_ER_IRQHandler */
.word DMA2D_IRQHandler /* DMA2D */
.size g_pfnVectors, .-g_pfnVectors
2024-05-31 06:05 AM
I've looked even deeper into it, turns out this IRQn is 26, defined in IRQn_Type enum.
TIM1_TRG_COM_TIM11_IRQn = 26, /*!< TIM1 Trigger and Commutation Interrupt and TIM11 global interrupt */
The HAL_NVIC_EnableIRQ, calls NVIC_EnableIRQ with that number, which is a macro for
__STATIC_INLINE void __NVIC_EnableIRQ(IRQn_Type IRQn)
{
if ((int32_t)(IRQn) >= 0)
{
__COMPILER_BARRIER();
NVIC->ISER[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
__COMPILER_BARRIER();
}
}
Then here if I am not mistaking, we divide the number by 2^5 = 32, to find which ISERx register 32 bit words this number belongs to 26/32 = 0 so ISER0. Then we extract the lower 5 bits of 26 which is 26. And put one into bit 27 (if counting from bit 0).
That then corresponds to the following highlighted bit
ISER0 bit 27 set
I don't know how to see if there is some mismatch in the NVIC controller or something for why this is not firing. I hope I have provided enough information for anyone that would be able to help me :)
2024-05-31 07:01 AM
In your timer screenshots, TIMx_DIER=0x1, i.e. only UIE is set, not the commutation interrupt enable bit.
I don't use Cube/HAL.
JW
2024-05-31 07:47 AM - edited 2024-05-31 07:48 AM
Thank you very much JW, this was absolutely that problem. I would have thought that either it would be enabled through CubeIDE or through the
HAL_TIMEx_ConfigCommutEvent(&htim1, TIM_TS_NONE, TIM_COMMUTATION_SOFTWARE);
I was unaware of this register (DIER) DMA/Interrupt Enable Register. For anyone else that might stumble on a similar problem adding the second line below, enables the com interrupt for TIM1.
HAL_TIMEx_ConfigCommutEvent(&htim1, TIM_TS_NONE, TIM_COMMUTATION_SOFTWARE);
htim1.Instance->DIER |= TIM_DIER_COMIE; // THIS LINE!
Again thank you very kindly for the assistance JW, I was losing my hair :grinning_face_with_sweat:
2024-05-31 07:49 AM
But that has me wondering if there is some HAL function call missing, or if there is something wrong in the IDE pipeline. Because the UIE bit is set but not this one considering similar IDE setup.