2017-09-06 12:28 PM
A citation from 'RM0041. Reference manual. STM32F100xx':
OSSI: Off-state selection for Idle mode
This bit is used when MOE=0 on channels configured as outputs....0: When inactive, OC/OCN outputs are disabled (OC/OCN enable output signal=0).1: When inactive, OC/OCN outputs are forced first with their idle level as soon as CCxE=1 orCCxNE=1 (OC/OCN enable output signal=1).But. My experiments on
STM32F100RB have shown that this bit has no effect on the state of the outputs.
Can someone have an example of using the OSSI bit?
2017-09-07 04:37 PM
Hello!
Go to
and download the firmware.Inside , you can find an example using the Break Feature (and OSSI bit)
Regards
VF
2017-09-07 11:16 PM
This table is in RM0090 for the 'F4 and its second part (MOE=0) sheds some light on the OSSI issue:
In other words, if MOE=0 (which is the consequence of break input getting active, i.e. the ''something terrible happened, bail out'' mechanism engaged) you can chose if the outputs go threestate (when OSSI=0), or driven to a given state (see narrative there).
It appears that this table is incomplete in RM0041 - would like to know if on purpose or by mistake.
JW
2017-09-08 12:53 PM
Thank you all for helping me to solve my problem.
Vangelis Fortounas, in that example bit OSSI is set to 1:
...
sBreakConfig.OffStateIDLEMode = TIM_OSSI_ENABLE; ... HAL_TIMEx_ConfigBreakDeadTime(&TimHandle, &sBreakConfig); ...I would like to know the difference between the two modes (OSSI=0 and OSSI=1).
waclawek.jan, in my case, i could not get 'disabled state' at the output. I always get a 'idle' state, regardless of the OSSI bit (outputs OCx=OISx, OCxN=OISxN, except when simultaneously
OISx=not CCxP,
OISxN=not CCxNP).
2017-09-12 03:58 AM
Here is my code:
#include <stddef.h>
#include 'stm32f10x.h'
// Set state 'value' of bits of 'ref' by the mask.
template <typename T>
void assign_bit(T& ref, uint32_t mask, bool value){
if(value)
ref|=mask;
else
ref&=~mask;
}
// Set config. of TIM1.
void conf_tim1(bool moe, bool ossi, bool ossr,
bool ois1, bool ois1n,
bool cc1e, bool cc1ne, bool cc1p, bool cc1np,
bool oc1ref){
assign_bit(TIM1->BDTR, TIM_BDTR_OSSI, ossi);
assign_bit(TIM1->BDTR, TIM_BDTR_OSSR, ossr);
assign_bit(TIM1->CR2, TIM_CR2_OIS1, ois1);
assign_bit(TIM1->CR2, TIM_CR2_OIS1N, ois1n);
assign_bit(TIM1->CCER, TIM_CCER_CC1E, cc1e);
assign_bit(TIM1->CCER, TIM_CCER_CC1NE, cc1ne);
assign_bit(TIM1->CCER, TIM_CCER_CC1P, cc1p);
assign_bit(TIM1->CCER, TIM_CCER_CC1NP, cc1np);
// OC1M[2:0]=0x4 or OC1M[2:0]=0x5:
// force inactive level / force active level.
TIM1->CCMR1=((oc1ref)?0x5:0x4)<<4;
assign_bit(TIM1->BDTR, TIM_BDTR_MOE, moe);
}
void conf_tim1(uint32_t pack){
conf_tim1(pack&0x200, pack&0x100, pack&0x80,
pack&0x40, pack&0x20,
pack&0x10, pack&0x8, pack&0x4, pack&0x2,
pack&0x1);
}
int main(){
// Enable the necessary peripheral clock.
RCC->APB2ENR|=
RCC_APB2ENR_IOPAEN|
RCC_APB2ENR_IOPBEN|
RCC_APB2ENR_TIM1EN;
// PA8 (TIM1_CH1), PB13 (TIM1_CH1N):
// CNF.MODE=10=0xA (alt. out, push-pull, 2MHz max)
(GPIOA->CRH&=~0xF)|=0xA;
(GPIOB->CRH&=~(0xF<<(13-8)*4))|=0xA<<(13-8)*4;
// Try out possible combinations of configuration bits.
for(int i=0x000; i<=0x3FF; i++){
// Set configuration.
conf_tim1(i);
//Here we can check state of OC1, OC1N (PA8, PB13).
}
// Infinite loop
int j = 0;
while(true){
j++;
}
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2017-09-12 12:25 PM
Below are the results of execution of my program.
Control bitsOutput states (OC1, OC1N)
MOEOSSIOSSRCC1E*CC1NE*OIS1OIS1Nif CC1P, CC1NP =
= 00 = 01 = 10 = 11
0
x
x
x
x
0
0
00
00
00
11
0
1
01
01
10
01
1
0
10
01
10
10
1
1
00
11
11
11
* These bits must not be zero at the same time, as in accordance with the manual:
When both outputs of a channel are not used (CCxE = CCxNE = 0), the OISx, OISxN, CCxP and CCxNP bits must be kept cleared.
So, the timer always acts as if OSSI=1.
If MOE==0 then
OC1=OIS1,
OC1N=OIS1N,
except when J==1, where J=(OIS1 xor CC1P) and (OIS1N xor CC1NP).
In other words, J==1 when both values OIS1, OIS1N correspond to the active levels (not CC1P, not CC1NP).
Finally we have that OC1=OIS1 xor J, OC1N=OIS1N xor J.
The question is why the behavior of the timer with OSSI = 0 does not match the one described in the manual?
2017-09-12 03:06 PM
As I said, I quoted from the RM0090 manual, which is for the 'F4.
As I said there, that table is not completed in RM0041, and this may be intentional.
JW