cancel
Showing results for 
Search instead for 
Did you mean: 

TIM1 timer, register TIM1_BDTR, bit OSSI. What is the function?

Harry Hamper
Associate II
Posted on September 06, 2017 at 21:28

A citation from 'RM0041. Reference manual. STM32F100xx':

OSSI: Off-state selection for Idle mode

This bit is used when MOE=0 on channels configured as outputs.

...

0: When inactive, OC/OCN outputs are disabled (OC/OCN enable output signal=0).

1: When inactive, OC/OCN outputs are forced first with their idle level as soon as CCxE=1 or

CCxNE=1 (OC/OCN enable output signal=1).

But. My experiments on 

STM32F100RB have shown that this bit has no effect on the state of the outputs.

Can someone have an example of using the OSSI bit?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Posted on September 08, 2017 at 01:37

Hello!

Go to

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubef1.html

and download the firmware.

Inside , you can find an example using the Break Feature (and OSSI  bit)

0690X000006087AQAQ.png

Regards

VF

waclawek.jan
Super User
Posted on September 08, 2017 at 08:16

This table is in RM0090 for the 'F4 and its second part (MOE=0) sheds some light on the OSSI issue:

0690X000006087ZQAQ.png

In other words, if MOE=0 (which is the consequence of break input getting active, i.e. the ''something terrible happened, bail out'' mechanism engaged) you can chose if the outputs go threestate (when OSSI=0), or driven to a given state (see narrative there).

It appears that this table is incomplete in RM0041 - would like to know if on purpose or by mistake.

JW

Harry Hamper
Associate II
Posted on September 08, 2017 at 21:53

Thank you all for helping me to solve my problem.

Vangelis Fortounas, in that example bit OSSI is set to 1:

...

sBreakConfig.OffStateIDLEMode = TIM_OSSI_ENABLE;

...

HAL_TIMEx_ConfigBreakDeadTime(&TimHandle, &sBreakConfig);

...

I would like to know the difference between the two modes (OSSI=0 and OSSI=1).

waclawek.jan, in my case, i could not get 'disabled state' at the output. I always get a 'idle' state, regardless of the OSSI bit (outputs OCx=OISx, OCxN=OISxN, except when simultaneously

OISx=not CCxP, 

OISxN=not CCxNP).

Harry Hamper
Associate II
Posted on September 12, 2017 at 12:58

Here is my code:

#include <stddef.h>
#include 'stm32f10x.h'
// Set state 'value' of bits of 'ref' by the mask.
template <typename T>
void assign_bit(T& ref, uint32_t mask, bool value){
if(value)
ref|=mask;
else
ref&=~mask;
}
// Set config. of TIM1.
void conf_tim1(bool moe, bool ossi, bool ossr,
bool ois1, bool ois1n,
bool cc1e, bool cc1ne, bool cc1p, bool cc1np,
bool oc1ref){
assign_bit(TIM1->BDTR, TIM_BDTR_OSSI, ossi);
assign_bit(TIM1->BDTR, TIM_BDTR_OSSR, ossr);
assign_bit(TIM1->CR2, TIM_CR2_OIS1, ois1);
assign_bit(TIM1->CR2, TIM_CR2_OIS1N, ois1n);
assign_bit(TIM1->CCER, TIM_CCER_CC1E, cc1e);
assign_bit(TIM1->CCER, TIM_CCER_CC1NE, cc1ne);
assign_bit(TIM1->CCER, TIM_CCER_CC1P, cc1p);
assign_bit(TIM1->CCER, TIM_CCER_CC1NP, cc1np);
// OC1M[2:0]=0x4 or OC1M[2:0]=0x5:
// force inactive level / force active level.
TIM1->CCMR1=((oc1ref)?0x5:0x4)<<4;
assign_bit(TIM1->BDTR, TIM_BDTR_MOE, moe);
}
void conf_tim1(uint32_t pack){
conf_tim1(pack&0x200, pack&0x100, pack&0x80,
pack&0x40, pack&0x20,
pack&0x10, pack&0x8, pack&0x4, pack&0x2,
pack&0x1);
}
int main(){
// Enable the necessary peripheral clock.
RCC->APB2ENR|=
RCC_APB2ENR_IOPAEN|
RCC_APB2ENR_IOPBEN|
RCC_APB2ENR_TIM1EN;
// PA8 (TIM1_CH1), PB13 (TIM1_CH1N):
// CNF.MODE=10=0xA (alt. out, push-pull, 2MHz max)
(GPIOA->CRH&=~0xF)|=0xA;
(GPIOB->CRH&=~(0xF<<(13-8)*4))|=0xA<<(13-8)*4;
// Try out possible combinations of configuration bits.
for(int i=0x000; i<=0x3FF; i++){
// Set configuration.
conf_tim1(i);
//Here we can check state of OC1, OC1N (PA8, PB13).
}
// Infinite loop
int j = 0;
while(true){
j++;
}
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Harry Hamper
Associate II
Posted on September 12, 2017 at 21:25

Below are the results of execution of my program.

Control bitsOutput states (OC1, OC1N)

MOEOSSIOSSRCC1E*CC1NE*OIS1OIS1Nif CC1P, CC1NP =

= 00 = 01 = 10 = 11

0

x

x

x

x

0

0

00

00

00

11

0

1

01

01

10

01

1

0

10

01

10

10

1

1

00

11

11

11

* These bits must not be zero at the same time, as in accordance with the manual:

When both outputs of a channel are not used (CCxE = CCxNE = 0), the OISx, OISxN, CCxP and CCxNP bits must be kept cleared.

So, the timer always acts as if OSSI=1.

If MOE==0 then

OC1=OIS1,

OC1N=OIS1N,

except when J==1, where J=(OIS1 xor CC1P) and (OIS1N xor CC1NP).

In other words, J==1 when both values OIS1, OIS1N correspond to the active levels (not CC1P, not CC1NP).

Finally we have that OC1=OIS1 xor J, OC1N=OIS1N xor J.

The question is why the behavior of the timer with OSSI = 0 does not match the one described in the manual?

Posted on September 12, 2017 at 22:06

As I said, I quoted from the RM0090 manual, which is for the 'F4.

As I said there, that table is not completed in RM0041, and this may be intentional.

JW