cancel
Showing results for 
Search instead for 
Did you mean: 

THE STM32F446RE (Nucleo -64) in that the USART Does not receive the hex frame properly for MODBUS RTU.

Sprak.11
Associate II

In the Below mentioned image the HEX value which was transmitted by the controller is properly works

but while in the time of receiving the HEX Value from the terminal on that time it does not receive properly you can able to see that in picture I show the watch memory also.

please kindly help me to solve this problem

And kindly share details for handling MODBUS RTU with STM32.0693W000004KVUSQA4.png image

0 REPLIES 0