2018-08-08 08:56 AM
The *.stldr file generated by MX25LM51245G_STM32L4R9I-DISCO (@ ST-LINK Utility 4.2.0.0) can't work for STM32L4R9I-DISCO device.
Step1. According to the readme.txt in the directory of "C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\MX25LM51245G_STM32L4R9I-DISCO", The detail is as follows:
@par Example Description
This an example of an external loader of MX25LM51245G flash memory for STM32L4R9I-DISCO.
This loader can be used with STM32 ST-LINK Utility and STM32CubeProgrammer.
@par Hardware and Software environment
- This example runs on STM32L4R9xx devices.
- This example has been tested with STMicroelectronics STM32L4R9I-Discovery
boards and can be easily tailored to any other supported device
and development board.
@par How to use it ?
- Place the folder "MX25LM51245G_STM32L4R9I-DISCO" under the following path inside the STM32L4 Cube firmware package "STM32Cube_FW_L4_Vx.y.z" folder:
STM32Cube_FW_L4_Vx.y.z\Projects\STM32L4R9I_DISCO\Examples\OSPI
- Open your preferred toolchain
- Rebuild all files and load your image into target memory
- After build, the loader should be displayed in the external loaders window, ready-to-use.
Step2. Add Existing project of MX25LM51245G_STM32L4R9I-DISCO by using the EWARM 8.22.1,then rebuild all files.So the
*.out file will be generated, then rename to *.stldr and copy to the directory of "C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\"
IAR Configuration
Step3. When downloading MenuLauncher-STM32L4R9I-Discovery_V1.0.0.hex through ST-Link Utility 4.2.0.0,the error is as following:
23:49:29 : ST-LINK SN : 0678FF504955857567011028
23:49:29 : ST-LINK Firmware version : V2J29M18
23:49:29 : Connected via SWD.
23:49:29 : SWD Frequency = 4,0 MHz.
23:49:29 : Connection mode : Connect Under Reset.
23:49:29 : Debug in Low Power mode enabled.
23:49:29 : Device ID:0x470
23:49:29 : Device flash Size : 2MBytes
23:49:29 : Device family :STM32L4Rx
23:50:24 : [MenuLauncher-STM32L4R9I-Discovery_V1.0.0.hex] opened successfully.
Address Ranges [0x08000000 0x080001BC] [0x08006000 0x08006F48] [0x08007000 0x0803B303] [0x90000000 0x9022C30A]
23:50:24 : [MenuLauncher-STM32L4R9I-Discovery_V1.0.0.hex] checksum : 0x0F9EA60A
23:52:26 : Timeout during flash programming
23:52:26 : Error occured during erase operation!
Best Regards,
2018-08-10 07:17 AM
The default MX25LM51245G_STM32L4R9I-DISCO.stldr (156KB) provided by ST can work well. So I suspect that bug has existed in the source code of MX25LM51245G_STM32L4R9I-DISCO.
ST'ers, would you give the solution for solving the issue? Thanks.
2018-08-12 05:47 AM
Hello,ST'ers, would you give the solution for solving the issue? Thanks.
2018-08-15 08:13 AM
Hello,ST'ers, would you give the solution for solving the issue? Thanks.
2018-08-15 08:33 AM
There's not much presence from ST here, this is primarily user-driven forum.
You might want to use the support website https://my.st.com/ols or contact ST directly.
JW
2018-08-15 09:00 AM
I'm open to reasonable offers, but I'm not here to carry other peoples water. Resolving this will take time, effort and resources.
2018-08-19 01:19 PM
ST's code also say the 512 Mbit device is 32MB, rather than 64MB
2018-08-19 11:01 PM
@Community member
I‘ve got it. Thanks.
According to the datasheet of MX25LM51245G , the size of Flash is 64MB, rather than 32MB.
The *.stldr provided by ST (default) is only for 32MB external loader, perhaps because of artificial constraint.
2018-08-20 05:55 AM
Honestly I think this has more to do with the lack of thorough testing, and attention to detail.
2018-12-01 04:10 AM
Has anybody found a solution for that problem?
2018-12-01 04:20 AM
Yes, have several working loaders, really need hardware in hand, super hard to do blind.