the HAL has BUG of CAN drive on STM32F1?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-14 10:23 AM
Stm32F103 HAL_CAN_Transmit(&hcan,10) not working, always return HAL_TIMEOUT and HAL_ERROR, but when i use STD_Lib everything is good. So i think if the HAL has BUG of CAN on STM32F1?
Hello,
I'm trying to set up CAN on my STM32F103 to send a CAN message but I keep getting HAL_TIMEOUT error from the HAL_CAN_Transmit() function :
/* Check End of transmission flag */
while(!(__HAL_CAN_TRANSMIT_STATUS(hcan, transmitmailbox))) { /* Check for the Timeout */ if(Timeout != HAL_MAX_DELAY) { if((Timeout == 0U) || ((HAL_GetTick()-tickstart) > Timeout)) ///////here!!!!!!!!!!!!! { hcan->State = HAL_CAN_STATE_TIMEOUT;/* Cancel transmission */
__HAL_CAN_CANCEL_TRANSMIT(hcan, transmitmailbox);/* Process unlocked */
__HAL_UNLOCK(hcan); return HAL_TIMEOUT; } } }Here's my code:
/* Includes ------------------------------------------------------------------*/
&sharpinclude 'can.h'&sharpinclude 'gpio.h'
/* USER CODE BEGIN 0 */
CanTxMsgTypeDef TxMessage;CanRxMsgTypeDef RxMessage;/* USER CODE END 0 */CAN_HandleTypeDef hcan;
/* CAN init function */
void MX_CAN_Init(void){hcan.Instance = CAN1;
hcan.pTxMsg = &TxMessage; //????? hcan.pRxMsg = &RxMessage; hcan.Init.Prescaler = 6; hcan.Init.Mode = CAN_MODE_NORMAL; hcan.Init.SJW = CAN_SJW_1TQ; hcan.Init.BS1 = CAN_BS1_6TQ; hcan.Init.BS2 = CAN_BS2_5TQ; hcan.Init.TTCM = DISABLE; hcan.Init.ABOM = DISABLE; hcan.Init.AWUM = DISABLE; hcan.Init.NART = ENABLE; hcan.Init.RFLM = DISABLE; hcan.Init.TXFP = DISABLE; if (HAL_CAN_Init(&hcan) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }CAN_FilterConfTypeDef sFilterConfig;
// sFilterConfig.FilterNumber = 0; sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = 0x0000; sFilterConfig.FilterIdLow = 0x0000; sFilterConfig.FilterMaskIdHigh = 0x0000; sFilterConfig.FilterMaskIdLow = 0x0000; sFilterConfig.FilterFIFOAssignment = 0; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.BankNumber = 14;if (HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)
{ /* Filter configuration Error */ Error_Handler(); }}void HAL_CAN_MspInit(CAN_HandleTypeDef* canHandle)
{GPIO_InitTypeDef GPIO_InitStruct;
if(canHandle->Instance==CAN1) { /* USER CODE BEGIN CAN1_MspInit 0 *//* USER CODE END CAN1_MspInit 0 */
/* CAN1 clock enable */ __HAL_RCC_CAN1_CLK_ENABLE(); /**CAN GPIO Configuration PB8 ------> CAN_RX PB9 ------> CAN_TX */ GPIO_InitStruct.Pin = GPIO_PIN_8; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_PULLUP; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);__HAL_AFIO_REMAP_CAN1_2();
/* CAN1 interrupt Init */
HAL_NVIC_SetPriority(USB_LP_CAN1_RX0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USB_LP_CAN1_RX0_IRQn); /* USER CODE BEGIN CAN1_MspInit 1 *//* USER CODE END CAN1_MspInit 1 */
}}void HAL_CAN_MspDeInit(CAN_HandleTypeDef* canHandle)
{if(canHandle->Instance==CAN1)
{ /* USER CODE BEGIN CAN1_MspDeInit 0 *//* USER CODE END CAN1_MspDeInit 0 */
/* Peripheral clock disable */ __HAL_RCC_CAN1_CLK_DISABLE(); /**CAN GPIO Configuration PB8 ------> CAN_RX PB9 ------> CAN_TX */ HAL_GPIO_DeInit(GPIOB, GPIO_PIN_8|GPIO_PIN_9);/* CAN1 interrupt Deinit */
HAL_NVIC_DisableIRQ(USB_LP_CAN1_RX0_IRQn); /* USER CODE BEGIN CAN1_MspDeInit 1 *//* USER CODE END CAN1_MspDeInit 1 */
}}/* USER CODE BEGIN 1 */
u8 Can_Send_Msg(u8 i,u8* msg,u8 len){ u8 j=0; switch(i) { case 0:TxMessage.StdId = 0x200;break; case 1:TxMessage.StdId = 0x1FF;break; } TxMessage.IDE=CAN_ID_STD; // ??? TxMessage.RTR=CAN_RTR_DATA; // ??? TxMessage.DLC=len; // ???????? for(j=0;j<len;j++) TxMessage.Data[j]=msg[j]; if (HAL_CAN_Transmit(&hcan, 10) != HAL_OK) { /* Transmition Error */ Error_Handler(); } return 1; }u8 Can_Receive_Msg(u8 *buf)
{ u32 i;if((RxMessage.StdId|0x0F)==0x20F)
{ for(i=0;i<RxMessage.DLC;i++) buf[i] = RxMessage.Data[i]; buf[7] = RxMessage.StdId - 0x201; return RxMessage.DLC; } else return 0;}/***************RX????************/
void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef* hcan){ if (HAL_CAN_Receive_IT(hcan, CAN_FIFO0) != HAL_OK) { /* Reception Error */ Error_Handler(); } Can_Receive_Msg(RxMessage.Data);}/* USER CODE END 1 */#can-hal_can_transmit_it #bug? #stm32f1-halSolved! Go to Solution.
- Labels:
-
Bug-report
-
CAN
-
STM32F1 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 6:27 AM
I solved the problem.
it's a stupid reason. I set a wrong BITRATE of the CAN BUS of controller...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 3:05 AM
are you running a line driver ?
do you have at least two devices on the network ?
do you have a terminator on the bus ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 6:27 AM
I solved the problem.
it's a stupid reason. I set a wrong BITRATE of the CAN BUS of controller...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-15 7:23 AM
thank you for your reply. i use it to run a DC motor with speed controller.
i succeed by using StdPeriph_Lib ,but failed by HAL with CubeMX. So i think my hardware should be OK.
So, is there any other possible factor will cause
HAL_CAN_Transmit() Time out?
thx again for ur reply!