2024-02-02 03:43 AM - edited 2024-02-02 03:45 AM
I am using ST-LINK-V3 to flash my STM32G03 board.
I am using ST-LINK_CLI.exe tool (I have used it in the past without any issues).
I have built my firmware and generated .hex file. I then try to use the ST-LINK_CLI.exe tool as following:
```
C:\Users\my_user\tools\st_link>ST-LINK_CLI.exe -c SN=003500293532511031333430 -P My_proram -Rst
STM32 ST-LINK CLI v3.3.0.0
STM32 ST-LINK Command Line Interface
ST-LINK SN: 003500293532511031333430
ST-LINK Firmware version : V3J8M3B5S1
Connected via SWD.
Target voltage = 0.0 V
Connection mode: Normal
Reset mode: Software reset
Device ID: 0x466
Device flash Size: 32 Kbytes
Device family: STM32G0
Loading file...
Flash Programming:
File : My_program.hex
Address : 0x08000000
Memory programming...
▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒ 0%
The elf loader file is not accessible.
Unable to reset the MCU!
C:\Users\my_user\tools\st_link>
```
Why would it complain something about the elf loader file? I am not even using .elf format file.
I have noticed that this is quite a common issue with the ST-LINK_CLI but I haven't managed to find straight forward solution to this issue. Would highly appreciate if someone could shed some light
2024-02-02 04:24 AM
The internal / external flash loaders are .STLDR files in ELF format
STM32CubeProgrammer_v2.15.0\bin\FlashLoader\0x466.stldr
So it would need paths to the tools.
2024-02-02 05:14 AM - edited 2024-02-02 05:19 AM
Appreciate the response but is still not fully clear to me what is your suggested solution.
Do I need to modify my command (C:\Users\my_user\tools\st_link>ST-LINK_CLI.exe -c SN=003500293532511031333430 -P My_proram -Rst) in any way?
You have mentioned something about the STM32CubeProgrammer_v2.15.0\bin\FlashLoader\0x466.stldr however it is not fully clear what I am meant to do with this file? Do I need to copy/paste this to my directory from which I am using ST-LINK_CLI.exe ?
Additionally, why would I be able to flash some other STM32 boards that I have lying around and only have problem with this specific STM32G03 board?
2024-02-02 07:40 AM
@LPetr.1 ST-LINK utility is quite old, it does not know newer products. Have you tried STM32_Programmer_CLI.exe instead?
2024-02-02 10:27 AM
Its complaining about not finding the loader salient for your hardware. You weren't clear about what loader/elf files it related too, but each part has it's own piece of code that needs to be pushed into RAM to program the internal FLASH.
G0 DEVID = 0x466
Either you're not using the right tools, or the subdirectory structure doesn't reflect expectations. Thus it "can't find" or "can't load"
As Pavel indicates the "ST-LINK Utilities" are old, and don't support newer families like the G0, so you likely need to start by using the right tools.
A complete / full install of STM32 Cube Programmer is strongly suggested.
2024-02-02 12:13 PM
> A complete / full install of STM32 Cube Programmer is strongly suggested.
Or CubeIDE, because it includes STM32_Programmer_CLI with its MCU and boards database and the loaders up to date.
2024-02-04 09:45 PM
Using STM32_Cube_Programmer_CLI instead of the st-link_cle.exe seems to work without any issues.