cancel
Showing results for 
Search instead for 
Did you mean: 

the balance between data size and FIFO threshold stm32H743II boards

VKats.1
Associate II

Hi,

I am working with 2 boards (stm32H743II) - one defined as SPI Master with SPI4 block and the other as SPI Slave with SPI5 block.

I am trying to understand the balance between:

# Init.DataSize configuration and Init.FifoThreshold

can someone give me some examples that explain the balance between them?

this is the first time I am trying to develop an SPI slave block.

thank you

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

They are (mostly) independent settings.

Data size sets the number of bits per transaction (word size) and FIFO threshold adjusts the FTHLV field which adjust how much data is needed/required for the TXP/RXP flags get set.

If you feel a post has answered your question, please click "Accept as Solution".