cancel
Showing results for 
Search instead for 
Did you mean: 

TFM in u575 microcontroller

Istillaga
Associate III

Hello,


The TFM application that is based on the stm32u585 board could work for the stm32u575zit6 microcontroller? I have modified the TFM project and I have removed hw accelerator from the SBSFU project because the u575 microcontroller does not contain this peripheral but in the TFM_Appli application I get cryptographic errors when building the project.

Thanks in advance

1 REPLY 1
TDK
Guru

The STM32U575 doesn't have cryptographic functionality. If the project uses those features, it cannot be ported to that chip.

What errors do you get? Be specific with screenshots if possible.

If you feel a post has answered your question, please click "Accept as Solution".