cancel
Showing results for 
Search instead for 
Did you mean: 

TDA8026 smart card reader with B-U585I-IOT02A.

RK.15
Associate II

Hello ST,

I am trying to interface TDA8026 (NXP) smart card reader with B-U585I-IOT02A (STM32) and not sure how to proceed. Please let me know how this integration can be done.

Regards,

Rohit

3 REPLIES 3
Mohamed Aymen HZAMI
ST Employee

Hello @Community member​ and welcome to the community,

You can refer to the firmware example under this path " STM32Cube\Repository\STM32Cube_FW_U5_V1.1.1\Projects\STM32U575I-EV\Examples\SMARTCARD\SMARTCARD_ComDMA ".

you can download the firmware from here.

Mohamed Aymen

PJose.4
Senior

Hi @Community member​ 

Greetings

I am also having the same requirement

Were you able to find some info regarding porting STM32U585 with SAM Module TDA8026.

The above post is it similar to the SAM Module TDA8026.

Thanks

RK.15
Associate II

Hello @Mohamed Aymen HZAMI​

I wanted to know if SMARTCARD_ComDMA  example provide both T = 0 and T = 1 use cases ?. As I was refering AN4800 there is no mention of this example project. Please do let me know if there are any documentation associated with this example.

Regards,