cancel
Showing results for 
Search instead for 
Did you mean: 

STSW-LINK009 Driver Install Fail

alan29
Associate

Hello, 

I am on a MacBook Pro M2 running Parallels Windows 11. 

I have downloaded the STSW-LINK009 zip file. 

Because of my machine, I need to run the dpinst_amd64.exe file. It opens and runs perfectly fine but I am unable to install the drivers as it says "Install Failed" (Provided a screenshot below) 

Driver Install Fail.png

I have disabled the secure boot on Windows 11 to see if it helped, but it did not. 

I'm wondering if it's because these drivers are not compatible with my Mac M2, or if I need to take another route.

Any help will be amazing. Thank you. 

2 REPLIES 2
tnowroz
Associate II

Experiencing the same problem in my Microsoft Surface Pro 11 (ARM) laptop. Would highly appreciate a solution.

 

Tobe
Senior III

Why are you using win11?