cancel
Showing results for 
Search instead for 
Did you mean: 

STMFlashLoader Demo read protection

rich2399
Associate
Posted on June 03, 2015 at 05:50

Have been using the Discovery board with IAR tools for weeks now.  The board works find and I can program using STLink.  I would like to get the STMFlashLoader Demo or STMFlashLoader to work using UART3.  I have tried everything but both application indicated that I need to remove protection and I cannot seem to do that.

 All indications are that the applications are talking to the board.

Any suggestions for getting this to work?

#stm32f407-stmflashloader-discove
1 REPLY 1
Posted on June 03, 2015 at 15:18

How exactly do you have this wired up and to what pins? RS232 w/level conversion, USB-to-CMOS Serial?

Try using RealTerm, 9600 9E1 (Even Parity required), send 0x7F (hex) and see if you get the 0x79 response.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..