2011-05-20 4:52 AM
Hello,
I m trying to use the stm32vldiscovery board as a stand alone st-link programer, to program a stm32f207 microcontroller, through stm3220f board. As I plug the two board one to the other, before to start the debug session the stm32f2 (which is still runnning the old program) go quickly really warm. Anyone got these problem? I have checked the connection, but is there a need of any other wire? Thanks for your support.2011-05-20 5:16 AM
Did you remove the jumpers on the discovery board ? The user manual shows where these are. With the usb port pointing up, the jumpers are on the upper right. The connector to use for programming your stm32f207 is on the upper left. If your stm32f207 board is powered, just connect the ground, and swd signals.
2011-05-20 10:31 AM
Is the STM32F2 series even supported by the ST-LINK V1? The L and F2 series parts seem to be using the ST-LINK V2. And you should certainly be looking for the newest drivers.
http://www.st.com/internet/evalboard/product/251168.jsp Are the voltages compatible, and how do have it wired?2011-05-26 7:29 AM