cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5A9ZJY6QTR Pixel Resolution support

Ashu123
Associate

Hello all,
What is the pixel resolution support of STM32U5A9ZJY6QTR MCU.
I need support of 1080 x 1920 pixel resolution for max 6'' inch display with both MIPI DSI and RGB888 support.

Any possible help. 

2 REPLIES 2
STTwo-32
ST Employee

Hello @Ashu123 and welcome to the ST Community 😊.

I suggest you take a look at the AN4861 to calculate the supported resolution according to your project configurations. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

It doesn't have the bandwidth to support FHD resolution.

Perhaps can get to 1024x768.

You need memory for the frame buffer, perhaps two, and DSI/MIPI 2-Lane at 1Gbps total.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..